Shared/multiplexed storage media with i.MX8M Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Shared/multiplexed storage media with i.MX8M Mini

668 Views
craigeasdale
Contributor II

Hello,

I have a situation where I must access storage media from another system, which is also being written to constantly. I was thinking about using SDIO for this, but there is only one of these peripherals on each system. For this reason it makes sense to multiplex two identical SD/eMMC devices and switch them out quickly to allow the the i.MX8M system to copy a chunk of data from one device, while the other writes the next chunk of data to the other.

QDIwgLP

 

However, I need to understand what the limitations of the i.MX8M Mini to determine if this will work.

  1. What determines the SD card powering/mounting process?
  2. Can how SD cards are powered up/mounted be changed?
  3. Can the speed of SDIO be changed?
  4. Can I use SPI to access SD card data?

If anyone has another suggested approach for this problem I'd also be interested to hear it.

Labels (1)
0 Kudos
Reply
3 Replies

662 Views
igorpadykov
NXP Employee
NXP Employee

Hi Craig

 

>1.What determines the SD card powering/mounting process?
>2.Can how SD cards are powered up/mounted be changed?

 

seems only limitation on such configuration is power-up sequence described in

sect.3.2.1 Power-up sequence  i.MX 8M Mini Applications Processor Datasheet for Consumer Products


>3.Can the speed of SDIO be changed?

 

I am afraid not, as speed is defined automatically in SD driver when it reads SD capability register.

 

>4.Can I use SPI to access SD card data?

 

no.

 

Best regards
igor

0 Kudos
Reply

651 Views
craigeasdale
Contributor II

Hi Igor, thanks for your reply.

In table 30 of this document it talks about low speed/full speed/high speed mode (400KHz/25MHz/50MHz). What determines which clock frequency is used? And what is the default/max SDIO clock frequency?

 

Thanks,
Craig

0 Kudos
Reply

644 Views
igorpadykov
NXP Employee
NXP Employee

>What determines which clock frequency is used? 

 

driver reads CSD register of SD card and sets frequency accordingly.

Details can be found in SD specification on

https://www.sdcard.org/downloads/pls/

 

Best regards
igor

0 Kudos
Reply