Hi,
I looking for the configuration in which i.MX6 can capture a BT1120 1080i video on CSI parallel interface, compresses the video using VPU encoder and stream it over network.
The architecture will be :
=============== 16bit data bus =============
| | ====================> | | H.264 stream
| FPGA | pixel clock | i.MX6 | ===============> { IP Network }
| | ====================> | |
=============== =============
I have a few questions about this application:
Hi Isaac
1.3. it is not supported, one can look at below link with suggested solutions and port them
to necessary kernel (verified on iMX53 for both BT1120 progressive and BT1120 interlaced input,
IPU setting is same for iMX53 and iMX6)
Re: Patch to support adv7180 TVin chip for Freescale Android R10.4 BSP on iMX53 -blog archive
2.4. if you mean video encoding, it is supported by VPU module, IPU can not perform similar
on-the-fly compression. VPU usage is described in documentation included in Doc package
L3.14.28_1.0.0_iMX6QDLS_BUNDLE
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The provided patch at Re: Patch to support adv7180 TVin chip for Freescale Android R10.4 BSP on iMX53 -blog archive
seems to be for Android. Can it be applied to Kernel 3.10 BSP?
Is VPU compression supported for this input? (BT.1120 1920x1080 interlaced input on CSI Parallel)
suggest to look at presentation below for vpu capabilities