bitbaked meta-toolchain-qt
Install it with
~/yocto/build/tmp/deploy/sdk$ poky-eglibc-x86_64-arm-toolchain-qt-1.4.1.sh
Download Qtcreator from here http://qt-project.org/downloads
and Install it to Your home directory
edit the bin/qtcreator.sh
source /opt/poky/1.4.1/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi
#! /bin/shmakeAbsolute() {
case $1 in
/*)
# already absolute, return it
echo "$1"
;;
*)
# relative, prepend $2 made absolute
echo `makeAbsolute "$2" "$PWD"`/"$1" | sed 's,/\.$,,'
;;
esac
}....
To do it before "#! /bin/sh" is IMPORTANT!!!!
In QtCreator i set
Compiler as
/opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/armv7a-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++
Qt version as
/opt/poky/1.4.1/sysroots/x86_64-pokysdk-linux/usr/bin/qmake
sysroot as
/opt/poky/1.4.1/sysroots/armv7a-vfp-neon-poky-linux-gnueabi
Put them in a Kit

For connection to Your Board click on Device ---> Manage
Build a new project
and add some to the .pro file

add
TOOLCHAIN_HOST_TASK_append = " nativesdk-python-subprocess"
EXTRA_IMAGE_FEATURES = "debug-tweaks ssh-server-openssh"
to Your localconfig
bitbake core-image-sato-sdk
set a password to root via
ssh root@[boardip]
passwd
test connection via
sftp root@[boardip]
start qtcreator
./qtcreator.sh
Message was edited by: Joerg Boge
Nachricht geändert durch Joerg Boge Thanks to Diego Gonzalez
Dear Joerg-SH:
I using qmake to get the Makefile like this.
../../sysroots/i686-pokysdk-linux/usr/bin/qt5/qmake -spec ../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/lib/qt5/mkspecs/devices/linux-imx6-g++/ -o Makefile test.pro
It is no problem when i qmake.
But when i make my Makefile it will show the error like below:
arm-poky-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp -O2 -Wall -W -D_REENTRANT -fPIC -DQT_NO_DEBUG -DQT_WIDGETS_LIB -DQT_GUI_LIB -DQT_CORE_LIB -I. -I../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/qt5 -I../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/qt5/QtWidgets -I../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/qt5/QtGui -I../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/qt5/QtCore -I. -I. -I../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/lib/qt5/mkspecs/devices/linux-imx6-g++ -o main.o main.cpp
In file included from ../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/qt5/QtGui/qwindowdefs.h:37:0,
from ../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/qt5/QtWidgets/qwidget.h:37,
from ../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/qt5/QtWidgets/qmainwindow.h:37,
from ../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/qt5/QtWidgets/QMainWindow:1,
from mainwindow.h:4,
from main.cpp:1:
../../sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/qt5/QtCore/qglobal.h:39:21: fatal error: cstddef: No such file or directory
compilation terminated.
make: *** [main.o] Error 1
I'm using qt5.5 to develop my application and Ubuntu 14.04 for my OS.
I don't know why this will happened.
Please Help!
Dear Joerg,
When i build a QT sample on Kit Warp7 occurs error: "/usr/bin/ld: cannot find -lQt5Core"
I had edited qtcreator.sh: source /opt/poky/2.1.2/environment-setup-cortexa7hf-neon-poky-linux-gnueabi 
but error still occur.
Any solution?
Thank you,
Ta Si
Hi everibody, i work with cross-compiled with imx6, but i have a problem with qmake, i download de toolchain armv7a in this link Index of /releases/yocto/yocto-2.0/toolchain/x86_64/, but in the moment of run, don't create the qmake for cross-compiler, someones help me please, regards...
Hai Joerg ,
I followed your steps for the Qt creater configuration for yocto build.
I bitbake meta-toolchain-qt.
then installed the tool chain. and edit qt creator .sh as per the above step
I configure in my qt creator
Compiler as
/opt/poky/1.6.3/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++
Qt version as
/opt/poky/1.6.3/sysroots/x86_64-pokysdk-linux/usr/bin/qt5/qmake
sysroot as
/opt/poky/1.6.3/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi
But I get an error like could not start process.
I here by attach my error log please find out, and help me to solve this error
Regards
Sachu
Dear All:
source setup-environment
MACHINE=imx6qsabresd source fsl-setup-release.sh -b build -e fb
bitbake meta-toolchain-qt5
QT SDK build sucessful
Hello Joerg-SH
I follow your step to setup QT.
$cd /home/wangq/work/yocto/fsl-release-bsp/sources/poky
$source oe-init-build-env
$bitbake meta-toolchain-qt
But there were some errors.
| collect2: ld returned 1 exit status
| make[1]: *** [lto1] Error 1
| make[1]: Leaving directory `/home/wangq/work/yocto/fsl-release-bsp/sources/poky/build/tmp/work/x86_64-pokysdk-linux/gcc-crosssdk/4.8.2-r0/gcc-4.8.2/build.x86_64-linux.x86_64-pokysdk-linux/gcc'
| make: *** [all-gcc] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/wangq/work/yocto/fsl-release-bsp/sources/poky/build/tmp/work/x86_64-pokysdk-linux/gcc-crosssdk/4.8.2-r0/temp/log.do_compile.8418)
ERROR: Task 547 (/home/wangq/work/yocto/fsl-release-bsp/sources/poky/meta/recipes-devtools/gcc/gcc-crosssdk_4.8.bb, do_compile) failed with exit code '1'
And I want to know this file(poky-eglibc-x86_64-arm-toolchain-qt-1.4.1.sh) came from where? I am new to all of this and any help would be greatly appreciated. Thanks
Hello,
After "bitbake meta-toolchain-qt", I ran the script "poky-eglibc-x86_64-meta-toolchain-qt-cortexa9hf-vfp-neon-toolchain-qt-1.5.3.sh ", can you check if this script is in your /build/tmp/deploy/sdk/ directory?
Dear Dizon:
if i want get poky-eglibc-x86_64-meta-toolchain-qt-cortexa9hf-vfp-neon-toolchain-qt-1.5.3.sh
the current dir is ~/work/yocto/fsl-release-bsp
the step :
1:source setup-environment
2:MACHINE=imx6qsabresd source fsl-setup-release.sh -b build -e fb
3:bitbake meta-toolchain-qt
      is it right ?
Hello Qiang Wangq,
I actually used a somewhat different method, I just do ". setup-environment build-x11" and then go straight through "bitbake meta-toolchain-qt". Maybe you can try your method and update us with your results.
Thanks
Hi
There is something error in the execution bitbake meta-toolchain-qt command ,and I can not find this file(poky-eglibc-x86_64-arm-toolchain-qt-1.4.1.sh).
Maybe you can post the contents of /home/wangq/work/yocto/fsl-release-bsp/sources/poky/build/tmp/work/x86_64-pokysdk-linux/gcc-crosssdk/4.8.2-r0/temp/log.do_compile.8418, so we can see the error.
Thanks
Hello Joerg-SH and thank you for this guide. I am using Qt 3.3 have followed your steps to setup Qt creator, and I have a few questions:
1) In specifying the kit, in the compiler tab there is an option for specifying the compiler path and make path. For the compiler path, I used "/opt/poky/1.5.3/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++" but I do not know what to put into the make path, do I just put the normal directory for the make utility?
2) I am using the latest Qt and Qt Creator, but after "bitbake meta-toolchain-qt", I think the version for Qt located within the sysroots folder is 4.8.5. Would this be OK?
I am new to all of this and any help would be greatly appreciated. Thanks
Hi Joerg-SH,
Thanks for detailed explanation.
However I noticed that if SDK is installed at path other than default installation path then specifying Qt version in qtcreator doesn't work. I get "Invalid Qt Version" error.
I run qmake -query command and found that all variables point to default SDK installation path and not at where SDK is installed.
Do you have any idea how to solve this?
Regards,
Dipen Patel
Hi guys,
does the meta-toolchain-qt has support for phonon?
Hi Joreg / Everybody,
I follow the same exact step as mentioned above (with same version of QT creator) ,
but I endup getting ABI detection failed in QT version tab ( i selected qmake2) and it throws exception
I tried clean install many times, but each time its the same.
Any input on this regard will be highly appreciated.
Thanks
Hello Jay,
thats "normal" should work properly with that!
If not than should be the mistake on an other place.
regards
Joerg
Thank you very much Joreg, let me try and see if everything goes fine.
Thanks.
Hi Joreg,
Now I stumble on this when I try to build (QT creator 2.8)
The below thread indicated that the follwing env variables has to be set
http://qt-project.org/forums/viewthread/29456
Joreg, do you happen to know if its necessary to add variables in the project build option ?
Thank you .
There is no need to do that
only
edit the bin/qtcreator.sh
source /opt/poky/1.4.1/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi
#! /bin/sh
and start i with it
Got it, Thank you Joreg :smileyhappy: