Trying to bring up a new board (to get to a u-boot prompt).
Initially tried using uuu -b emmc <our bin-flash> generated using Yocto after porting files from the RPA file for the board/ddr combo.
We get the following on the host running uuu:
\image>uuu -v -b emmc imx-boot-imx8mn-ddu-sd.bin-flash_evk
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.149-6-gd82f8f1
Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDPS: MX8ULP 0x1fc9 0x014a
SDPS: MX8ULP 0x1fc9 0x014b
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
Run built-in script:
uuu_version 1.2.39
# @_flash.bin | bootloader
# @_image [_flash.bin] | image burn to emmc, default is the same as bootloader
# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8mn-ddu-sd.bin-flash_evk
# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f imx-boot-imx8mn-ddu-sd.bin-flash_evk
# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8mn-ddu-sd.bin-flash_evk -offset 0x57c00
SDPU: jump
# }
# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8mn-ddu-sd.bin-flash_evk -skipspl
SDPV: jump
# }
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash bootloader imx-boot-imx8mn-ddu-sd.bin-flash_evk
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: Done
Wait for Known USB Device Appear...
New USB Device Attached at 1:1
1:1>Start Cmd:SDPS: boot -f imx-boot-imx8mn-ddu-sd.bin-flash_evk
5%1:1>Fail HID(W):LIBUSB_ERROR_TIMEOUT(1.035s)
On the serial port, watching the process we get:
U-Boot SPL 2021.04-5.10.35-2.0.0+gc604cd7739 (Dec 13 2021 - 16:42:58 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3200MTS
Training FAILED
This looked to me like the DDR is not being configured properly. So I used the Config Tools for iMX (v10.0) DDR tool and the RPA for the memory with the board to try testing the memory configuration.
The Fimware Init and Operational tests are passing fine.
I then rebuilt u-boot-imx with the files produced using the DDR tool and tried to use the uuu manufacturing tool to load the image.
The board is giving me the same failures.
已解决! 转到解答。
Hi @amberworth,
As for your questions:
1. How should we directly load the emmc of the new board with the uuu manufacturing tool?
Please refer to the document I sent you directly could help you, but as the way you are doing seems correct.
2. Is there an additional configuration step need somewhere to configure the system to use the DDR4 memory on the board? (How do you configure the emmc so that the system can boot to u-boot with a custom board?)
Take a look on the next document, can give you an Idea on how to do it.
3. Since the Config Tools for iMX DDR tool is able to read and write, is there a way to leverage this to write an inital u-boot to the board?
Unfortunate no, as the tool just write and read from the DDR and not for the eMMC or SD memory.
There is other way to build the DDR source code, using the DDR tool, you can find all the info on the next link, in the case you one give it a try:
i.MX 8M Family DDR Tool Release - NXP Community
Regards,
Israel.
Hi @amberworth,
As for your questions:
1. How should we directly load the emmc of the new board with the uuu manufacturing tool?
Please refer to the document I sent you directly could help you, but as the way you are doing seems correct.
2. Is there an additional configuration step need somewhere to configure the system to use the DDR4 memory on the board? (How do you configure the emmc so that the system can boot to u-boot with a custom board?)
Take a look on the next document, can give you an Idea on how to do it.
3. Since the Config Tools for iMX DDR tool is able to read and write, is there a way to leverage this to write an inital u-boot to the board?
Unfortunate no, as the tool just write and read from the DDR and not for the eMMC or SD memory.
There is other way to build the DDR source code, using the DDR tool, you can find all the info on the next link, in the case you one give it a try:
i.MX 8M Family DDR Tool Release - NXP Community
Regards,
Israel.