Setting up a 7 in touch lcd (800x480) with IMX8 MINI (imx8mmevk) in Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting up a 7 in touch lcd (800x480) with IMX8 MINI (imx8mmevk) in Yocto

898 Views
Alirezah95
Contributor II

Hi 

I have a Yocto image for imx8 mini with the wayland and weston and I'm trynig to set up a 7 inch HDMI touch LCD with 800x480 resolution as the display, but no success so far. The image is working fine in HDMI FullHD display though.

I should also mention that in the above LCD we have the NXP icon at the begining of the Yocto image and also when the image boots up the screen turns white which I believe is because of the app I've set to run on the board using services. So it seems that weston is running but the render resolution is larger than 800x480 and it seems that only a part of the contents are being displayed.

How can I fix this problem?

0 Kudos
Reply
1 Reply

846 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have to create a driver for that resolution this may help:

https://github.com/ArashEM/meta-mangopi

 

Regards

0 Kudos
Reply