Setting up Wl18xx in linux 3.14.28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting up Wl18xx in linux 3.14.28

1,527 Views
shree97
Contributor II

I want to set up the WiFi and Bluetooth(WL1835) on our custom board, where also it is connected to SD2 interface(WiFi) and UART2(BT). Now my question is I have drivers in the kernel 3.14.28 for wlcore, wl18xx and bluetooth ,will this driver code will work or I need to modify something?

If I need to modify then what part of the driver I need to modify?

Do I need to make changes in Device tree ?

Can I access the WiFi at u-Boot level, if yes then How?

Labels (3)
0 Kudos
Reply
6 Replies

881 Views
shree97
Contributor II

What changes I need to do in the Device Tree File ?

If you have any sample device tree file with related changes , plz. share with me.

                                                                                                                                     Thank You.

0 Kudos
Reply

881 Views
igorpadykov
NXP Employee
NXP Employee

one can follow 3.10.53 bring-up steps

Step-by-step: How to setup TI Wilink (WL18xx) with iMX6 Linux 3.10.53

Best regards

igor

0 Kudos
Reply

881 Views
shree97
Contributor II

Thanks for Reply.

They have given the description for 2.6 kernel but

I want to set up in 3.14.28

On Fri, May 6, 2016 at 4:21 PM, igorpadykov <admin@community.freescale.com>

0 Kudos
Reply

881 Views
shree97
Contributor II

But After that it requires to apply patches and I don't know which patches to apply?

0 Kudos
Reply

881 Views
LuisCasado
NXP Employee
NXP Employee
0 Kudos
Reply

881 Views
shree97
Contributor II

Thanks for Reply.

I have that modules with me but I just want to know do I need to modify the driver codes?

because while traversing driver code I am unable to find pin related info

0 Kudos
Reply