Hi
I have installed ubuntu onto my SabreSD evaluation board. In the command line parameters I specify that the monitor I'm using is 1280x1024, but when Ubuntu boots the screen is stuck at 640x480, there's nothing I can do to change it. The settings program does not allow me to change the resolution, I've tried using xrandr -addmode mxcfb0 1280x1024 and used hdmi instead of mxcfb0 but had no success, I just got a message saying it could not find the output specified.
The command line I specify in the uboot environment is
setenv bootargs_mmc setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb0:dev=hdmi,1280x1024M@60,if=RGB24 video=mxcfb1:off video=mxcfb2:off fbmem=28M ip=dhcp
I have used the monitor on another system at 1280x1024 so I know it should work.
What do I need to do to change the screen resolution in ubuntu?
Incidently I have the same issue when running Android as supplied with the kit.
Kind regards
Andrew
已解决! 转到解答。
Hi Michel,
If I connect a a DVI monitor with an HDMI DVI cable then typing the following command:
cat /sys/class/graphics/fb0/modes
Yields:
V:640x480p-60
U:640x480p-60
It would appear the a monitor with a DVI interface is not being interrogated properly so ubuntu defaults to the above mode. I have repeated the above test with a TV with HDMI and it yielded the following modes:
S:1920x1080p-24
S:720x576p-50
S:720x480p-60
S:1280x720p-50
S:1280x720p-60
S:1920x1080p-50
S:1920x1080p-60
V:640x480p-60
D:1920x1080p-60
U:640x480p-60
Firstly how can I configure ubuntu to default to a higher resolution and how do I make ubuntu recognise a DVI device?
Andrew
Hi again,
I have added some printks to my code to observer what is happening at boot up the output I've got is shown below:
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver hdmi
mxc_hdmi_disp_init
mxc_hdmi mxc_hdmi: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: 1280x1024@60: CVT Name - 1.310M4
imx-ipuv3 imx-ipuv3.0: WARNING: adapt panel end blank lines
imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
imx-ipuv3 imx-ipuv3.0: WARNING: adapt panel end blank lines
Console: switching to colour frame buffer device 160x64
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
mxc_sdc_fb mxc_sdc_fb.1: Can't get fb option for mxcfb1!
mxc_sdc_fb mxc_sdc_fb.2: Can't get fb option for mxcfb2!
mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb
mxc_hdmi_read_edid
mxc_edid_read
_regulator_get: get() with no identifier
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
imx-sdma imx-sdma: loaded firmware 1.1
Display is GTF capable
mxc_hdmi_read_edid: modes found
mxc_edid_mode_to_vic xres: 1280 yres: 1024
mxc_edid_mode_to_vic xres: 720 yres: 400
mxc_edid_mode_to_vic xres: 640 yres: 480
mxc_edid_mode_to_vic xres: 640 yres: 480
mxc_edid_mode_to_vic xres: 640 yres: 480
mxc_edid_mode_to_vic xres: 640 yres: 480
mxc_edid_mode_to_vic xres: 800 yres: 600
mxc_edid_mode_to_vic xres: 800 yres: 600
mxc_edid_mode_to_vic xres: 800 yres: 600
mxc_edid_mode_to_vic xres: 800 yres: 600
mxc_edid_mode_to_vic xres: 832 yres: 624
mxc_edid_mode_to_vic xres: 1024 yres: 768
mxc_edid_mode_to_vic xres: 1024 yres: 768
mxc_edid_mode_to_vic xres: 1024 yres: 768
mxc_edid_mode_to_vic xres: 1280 yres: 1024
mxc_edid_mode_to_vic xres: 1280 yres: 1024
mxc_edid_mode_to_vic xres: 1152 yres: 864
mxc_edid_mode_to_vic xres: 1280 yres: 960
mxc_edid_mode_to_vic xres: 640 yres: 512
mxc_edid_mode_to_vic xres: 640 yres: 360
mxc_edid_mode_to_vic xres: 720 yres: 405
fbcvt: 1280x1024@60: CVT Name - 1.310M4
imx-sdma imx-sdma: initialized
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
FB_EVENT_MODE_CHANGE
mxc_hdmi_setup
mxc_hdmi_setup: DVI mode
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
mxc_hdmi_fb_event HDMI device mxc_hdmi ID -1
FB_EVENT_MODE_CHANGE
mxc_hdmi_setup
mxc_edid_mode_to_vic xres: 640 yres: 480
mxc_hdmi_setup: DVI mode
console [ttymxc0] enabled, bootconsole disabled
It appears that information about the display is being overwritten. To begin with it can be seen that a range of modes are being found from the display, then the mode information is being erased and replace with 640x480. I'm not yet sure whats going on. Does anyone have anyideas as to what is happening?
Andrew
Hi Michel,
I'm using L3.0.35_1.1.0_121218, which is the latest version available on the website.
Have you been able to verify that this version works with a DVI monitor using an HDMI to DVI converter cable?
Thanks
Andrew
We have reproduced the issue. Apparently it only happens when using a HDMI to DVI cable.
I'm trying to get a solution for this problem but it would be a better idea to simply use a HDMI to HDMI cable.
Michel