Setting options for imxvpuenc_h264

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting options for imxvpuenc_h264

956 Views
brainmeltdown
Contributor I

I need to program the imxvpuenc_h264 Gstreamer plugin in C for use with RTP.  Where do I find documentation for options like those I have seen in other posts such as gop-size and bitrate?  I know I will almost certainly have to set slice sizes or max NAL sizes somehow.  

Labels (4)
0 Kudos
Reply
1 Reply

669 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mike

imxvpuenc_h264 is part gstreamer-imx plugins developed and supported

by community, it may be posted on meta-fsl-arm mailing list, so that someone familiar

with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

difference between community gstreamer-imx plugins and nxp gstreamer plugins described on

trac.gateworks.com/wiki/Yocto/gstreamer

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply