Setting of G-Ethernet PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting of G-Ethernet PHY

Jump to solution
1,322 Views
eishishibusawa
Contributor III

Dear Sir

 

Please tell me about pin processing of the MCIMX6SX SDB G-Ethernet.

I refer to the SCH-27962 PDF: SPF-27962 Rev.C.

 

Q1.

Is the voltage of NVCC_RGMII 1.5V?

 

I think that the Supply voltage of RGMII I/O has the following settings.

1.5V

1.8V

2.5V

3.3V

Q2.

How should we choose the voltage for RGMII I/O?

Please tell me the difference of behavior at each voltage.

 

Customer is considering to adopt the KSZ9031RNX(MicroChip).

Q3.

Is it able to use the KSZ9031RNX with i.MX6SoloX?

 

Best Regards,

Eishi SHIBUSAWA

Labels (1)
0 Kudos
Reply
1 Solution
1,221 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

>Q1. Is the voltage of NVCC_RGMII 1.5V?

yes

>I think that the Supply voltage of RGMII I/O has the following settings.

>・1.5V  1.8V 2.5V 3.3V

right

>Q2.How should we choose the voltage for RGMII I/O?

>Please tell me the difference of behavior at each voltage.

there is no difference in behaviour or performance using these voltages,

it should be choosed based on rgmii phy datasheet requirements.

>Q3.Is it able to use the KSZ9031RNX with i.MX6SoloX?

KSZ9031RNX has VDDIO 3.3V, 2.5V, or 1.8V so it is supported by i.MX6SoloX.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,222 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

>Q1. Is the voltage of NVCC_RGMII 1.5V?

yes

>I think that the Supply voltage of RGMII I/O has the following settings.

>・1.5V  1.8V 2.5V 3.3V

right

>Q2.How should we choose the voltage for RGMII I/O?

>Please tell me the difference of behavior at each voltage.

there is no difference in behaviour or performance using these voltages,

it should be choosed based on rgmii phy datasheet requirements.

>Q3.Is it able to use the KSZ9031RNX with i.MX6SoloX?

KSZ9031RNX has VDDIO 3.3V, 2.5V, or 1.8V so it is supported by i.MX6SoloX.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply