Setting mx8mq frequency lower than 800MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting mx8mq frequency lower than 800MHz

873 Views
alexandru_costa
Contributor I

Hi,

Is it possible to clock the mx8mq lower than 800MHz? By default the governor only allows for choosing between 1 and 1.5GHz

By editing the grades in imx8mqevk/kernel-source/drivers/soc/imx/soc-imx8.c it now allows setting the cpu freq as low as 800Mhz.

Would it be possible to clock it lower than that and if yes, can you help with an example for Kernel 4.14.98?

Thank you

0 Kudos
Reply
1 Reply

862 Views
igorpadykov
NXP Employee
NXP Employee

Hi alexandru_costa

 

one can try to tweak dts "&A53_0 { operating-points.."

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8mq-e...

and use CPU Frequency Scaling (CPUFREQ) Linux Chapter of Reference Manual in

Documentation

 

Best regards
igor

0 Kudos
Reply