Set i.MX8X to Partial Field Return lifecycle status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Set i.MX8X to Partial Field Return lifecycle status

ソリューションへジャンプ
1,392件の閲覧回数
gonzalo_ruiz
Contributor II

Hello NXP team,

I have an i.MX8X unit in "OEM Closed" state and I want to return it to "Partial Field Return" state. For that I am using the SCU API to send the SECO_FUNC_RETURN_LIFECYCLE from the A-core CPU to the SECO, but I am having problems with the message whose address I have to send as parameter.

Documentation says it should be a message signed by OEM SRK. I tried loading a binary file signed with OEM SRKs to RAM and then use the RAM address as parameter of that SCU function, but it failed with a SC_ERR_PARM (Bad parameter) error. I tried authenticating the file and it works fine.

=> auth_cntr $loadaddr
Authenticate OS container at 0x88280000
  Authenticate image from DDR location 0x88280000... OK

Is there a specific message expected by the SECO? Can you tell me how can I create it?

Regards,

Gonzalo

0 件の賞賛
返信
1 解決策
1,379件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately there is no public information we can share through here, would recommend to proceed with professional services for this:
https://contact.nxp.com/new-prof-svcs-sw-tech

Best regards,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,380件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately there is no public information we can share through here, would recommend to proceed with professional services for this:
https://contact.nxp.com/new-prof-svcs-sw-tech

Best regards,
Aldo.

0 件の賞賛
返信