Set Quality of vpuenc mjpg?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set Quality of vpuenc mjpg?

5,113 Views
gavingreenwalt
Contributor III

Is there a way to adjust the quality of the mjpg VPU encoder through gstreamer or is the hardware mjpg quality unchangeable?  I tried changing quant but saw no effect.

Labels (2)
0 Kudos
Reply
17 Replies

2,552 Views
rajasekarmuruge
Contributor I

Hi,

   Any patch is available to achieve various bitrates with mjpeg codec? I've tried with unit test program, file size remains the same. Any suggestions for this? I'm using gstreamer-0.1.

0 Kudos
Reply

2,552 Views
gavingreenwalt
Contributor III

This is really holding me up.  Is it or is it not impossible to adjust qualityof MJPEG encode?  I can't stream somewhere between 5 and 30mbps 720p depending on the image.  I need a semi-constant bitrate.   I tried VBR and CBR (0 and 1) I tried quantParam and bitRate and nothing changed.

0 Kudos
Reply

2,552 Views
igorpadykov
NXP Employee
NXP Employee

iisue was elevated to app team and below feedback from experts:

----------------------------------------

You only have access to few parameters listed when you use

$ gst-inspect vpuenc

make sure you focus on one gst only (gst1.0 OR gst0.1)

If you find some supported command line which produces inconscistent result, please, share here and I can work to reproduce.

Oh, another important question, BSP release version and freescale reference board?

----------------------------------------

Best regards

igor

0 Kudos
Reply

2,552 Views
timharvey
Contributor IV

Yuri,

From what I've found the bitrate and quant value to vpuenc has no effect what-so-ever for the JPEG codec, and I would assume this is simply a limitation of the codec within the vpudec firmware. It doesn't matter what version of gstreamer, gst-fsl-plugins, or vpulib I use. It appears to have the desired effect for all other codecs (MPEG4, H264, H263), just not JPEG.

If you can prove me wrong, I would be love to hear exactly what software you are using and what gst-launch pipeline you are using.

Regards,

Tim

0 Kudos
Reply

2,551 Views
Yuri
NXP Employee
NXP Employee

Please let me look at log of command

$ gst-inspect vpuenc

Regards,

Yuri.

0 Kudos
Reply

2,551 Views
timharvey
Contributor IV

Yuri,

# gst-inspect vpuenc

Factory Details:

  Long name:    VPU-based video encoder

  Class:        Codec/Encoder/Video

  Description:  Encode raw video to compressed data by using VPU

  Author(s):    Multimedia Team <shmmmw@freescale.com>

  Rank:        primary + 1 (257)

Plugin Details:

  Name:                vpu.imx

  Description:          VPU-based video codec

  Filename:            /usr/lib/gstreamer-0.10/libmfw_vpu.so

  Version:              3.0.11

  License:              LGPL

  Source module:        gst-fsl-plugins

  Binary package:      Freescle Gstreamer Multimedia Plugins

  Origin URL:          http://www.freescale.com

GObject

+----GstObject

      +----GstElement

            +----GstVpuEnc

Pad Templates:

  SINK template: 'sink'

    Availability: Always

    Capabilities:

      video/x-raw-yuv

                format: TNVP

      video/x-raw-yuv

                format: NV12

      video/x-raw-yuv

                format: I420

  SRC template: 'src'

    Availability: Always

    Capabilities:

      video/mpeg

            mpegversion: 4

          systemstream: false

      video/x-h263

      video/x-h264

      image/jpeg

Element Flags:

  no flags set

Element Implementation:

  Has change_state() function: gst_vpuenc_state_change

  Has custom save_thyself() function: gst_element_save_thyself

  Has custom restore_thyself() function: gst_element_restore_thyself

Element has no clocking capabilities.

Element has no indexing capabilities.

Element has no URI handling capabilities.

Pads:

  SRC: 'src'

    Implementation:

      Has custom eventfunc(): gst_vpuenc_src_event

      Has custom queryfunc(): gst_pad_query_default

      Has custom iterintlinkfunc(): gst_pad_iterate_internal_links_default

      Has getcapsfunc(): gst_pad_get_fixed_caps_func

      Has acceptcapsfunc(): gst_pad_acceptcaps_default

    Pad Template: 'src'

  SINK: 'sink'

    Implementation:

      Has chainfunc(): gst_vpuenc_chain

      Has custom eventfunc(): gst_vpuenc_sink_event

      Has custom queryfunc(): gst_pad_query_default

      Has custom iterintlinkfunc(): gst_pad_iterate_internal_links_default

      Has bufferallocfunc(): gst_vpuenc_alloc_buffer

      Has setcapsfunc(): gst_vpuenc_setcaps

      Has acceptcapsfunc(): gst_pad_acceptcaps_default

    Pad Template: 'sink'

Element Properties:

  name                : The name of the object

                        flags: readable, writable

                        String. Default: "vpuenc0"

  codec              : The codec type for encoding

                        flags: readable, writable

                        Enum "vpuenc_codec" Default: 0, "mpeg4"

                          (0): mpeg4            - video/mpeg, mpegversion=(int)4, systemstream=(boolean)false

                          (5): h263            - video/x-h263

                          (6): avc              - video/x-h264

                          (12): mjpg            - image/jpeg

  seqheader-method    : (0)auto; (1)send in codec_data of caps; (2)send with first buffer; (3)always send codec_data with buffers

                        flags: readable, writable

                        Integer. Range: 0 - 3 Default: 0

  timestamp-method    : (0)use input buffer's timestamp; (1)use GST_CLOCK_TIME_NONE

                        flags: readable, writable

                        Integer. Range: 0 - 1 Default: 0

  cbr                : constant bitrate

                        flags: readable, writable

                        Boolean. Default: true

  bitrate            : set bit rate in bps, valid only when cbr is true, 0: auto

                        flags: readable, writable

                        Integer64. Range: 0 - 2147483647 Default: 0

  gopsize            : set number of frame in a gop

                        flags: readable, writable

                        Integer. Range: 1 - 2147483647 Default: 15

  quant              : set quant value, valid only when cbr is false: H.264(0-51), Mpeg4/H.263(1-31), -1:auto

                        flags: readable, writable

                        Integer. Range: -1 - 51 Default: -1

  framerate-nu        : set framerate numerator

                        flags: readable, writable

                        Integer. Range: 1 - 2147483647 Default: 30

  framerate-de        : set framerate denominator

                        flags: readable, writable

                        Integer. Range: 1 - 2147483647 Default: 1

  force-framerate    : enable force fixed framerate for encoding

                        flags: readable, writable

                        Boolean. Default: false

I see nothing above that tells me that MJPG doesn't support varied bitrates (it does seem to indicate perhaps that quant isn't support for MJPG).

So again, I ask the simple question: Does gst-fsl-plugins vpuenc support a quality/bitrate property that ultimately varies the outputted framesize and if not where is the limitation? From my testing vpuenc supports varying bitrate/quant to produce output frames that vary in size for other codes so I believe this is a limitation of the vpu firmware itself.

Tim

0 Kudos
Reply

2,552 Views
Yuri
NXP Employee
NXP Employee

  It looks like  gstreamer 0.10 is used in the case.

Would You please use only gstreamer 1.0 ?

We have been suggested by multimedia team to only

use gstreamer 1.0 because they are going to finish the

gst0.1 support.

Regards,

Yuri.

0 Kudos
Reply

2,552 Views
timharvey
Contributor IV

Yuri,

The same behavior occurs with gst1.0.

I feel like we are going in circles here. If you feel that the MJPG vpuenc codec with gst-fsl-plugins really does allow variable bitrate support as seems to be indicated by all documentation I've read, please show me exactly what gstreamer pipeline and software versions you are using and demonstrate to me that it works (your choice of software, your choice of hardware - I'll figure out the differences if I have a known good scenario to work from).

Regards,

Tim

0 Kudos
Reply

2,552 Views
Yuri
NXP Employee
NXP Employee

Please see the last message from MM team

For vpu mjpeg encoder, customer need to set related parameter table to adjust the quality.

Related api includes:

encop.EncStdParam.mjpgParam.mjpg_qMatTable=...

vpu_EncOpen(&handle, &encop);

There is already one default table in freescale's vpu unit test, customer can adjust the quality through scaling it.

Customer can refer to jpeg specification for more details.

So, if one needs to have this setup via gstreamer, they can change its source code.

The  unit tests and the VPU user guide can help here.

Unfortunately, it looks like we have an pointless plugin parameter, however, in other hand,

the parameter is already there, customers decide if they need to implement it and how.

0 Kudos
Reply

2,552 Views
byc013
Contributor I

Hello,

I am facing the same challenge as you guys do. Trying to stream JPEGs (MJPEG) over UDP, but JPEG frames are too big and thus being dropped by the udpsink.

Please clarify: The parameters aren't implemented in gst-fsl-plugin level or in VPU firmware level?

If the new implementation should be in firmware level, would it be about changing/recompiling the /lib/firmware/vpu/vpu_fw_imx6d.bin?

I am a Linux software developer and I must say that this is really frustrating for me since this kind of development is out of my scope and is blocking my progress.

Does anyone have any patch or something that can help to control the JPEG compression?

Thanks,

Yechiel

0 Kudos
Reply

2,552 Views
timharvey
Contributor IV

Yechiel,

Correct - gst-fsl-plugins does not implement the ability to alter the JPEG quality. The 'fix' would need to go into the vpulib by adding multiple quantization tables and selecting one based on the quality parameter passed up through the plugin.

This feature is also missing from the gstreamer-imx plugins (which I feel are a much better solution for IMX6 IPU/VPU/GPU hardware acceleration in Gstreamer) but again, its not really an issue with the plugins but the wrapper around the VPU that they use.

Tim

0 Kudos
Reply

2,552 Views
Yuri
NXP Employee
NXP Employee

Tim, hello !

Looks like the quality parameters do not work for MJPG, I will inform

the team about it.

Regards,

Yuri.

0 Kudos
Reply

2,552 Views
Yuri
NXP Employee
NXP Employee

In order to control size of JPEG stream one can use compress ratio:

  For VBR(bitRate=0): user can set proper 'quantParam' value to control the quality

less value, better quality, higher bitrate.

  For CBR(bitRate>0): user can set proper 'bitRate' value to control the quality

higher value, better quality.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,552 Views
timharvey
Contributor IV

Yuri,

This appears to not work using gst-fsl-plugin (4.0.3 or earlier 3.0.11) and can be shown via the following pipelines:

gst-launch videotestsrc num-buffers=1 ! vpuenc codec=mjpg cbr=false bitrate=0 quant=10 ! filesink location=/tmp/test.jpg && ls -l /tmp/test.jpg # yeilds a 9315 byte file every time

gst-launch videotestsrc num-buffers=1 ! vpuenc codec=mjpg cbr=true bitrate=100 quant=10 ! filesink location=/tmp/test.jpg && ls -l /tmp/test.jpg # yeilds a 9315 byte file every time

It doesn't seem to matter what params I provide for cbr, bitrate, or quant - it always results in a 9315 byte file

Tim

partner

gateworks

KevinWong

0 Kudos
Reply

2,552 Views
gavingreenwalt
Contributor III

I tried bitrate in the gst-launch-0.10 however it didn't change the datarate.  Is this only available through the library?

0 Kudos
Reply

2,552 Views
gavingreenwalt
Contributor III

bump?  I've tried bitrate and quant and neither affected the bitrate of the stream.

0 Kudos
Reply

2,552 Views
gavingreenwalt
Contributor III

Bump?

0 Kudos
Reply