Serial output is garbled [i.MX28EVA)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial output is garbled [i.MX28EVA)

913件の閲覧回数
uuffmm
Contributor I

I am trying the i.MX287 evaluation board as per reference manual. It is quite smooth. But I came across the following problem:   the Com1 output becomes garbled after decompressing the Linux kernel.

Please see my screen capture: The following is the printout of environment variables:

------------------------------Env. Variables ---------------------------

MX28 U-Boot > pri
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p3 rw rootwait ip=dhcp fec_mac=${ethaddr}
bootcmd_mmc=run bootargs_mmc; mmc read 0 ${loadaddr} 100 3000; bootm
ethact=FEC0
nfsroot=/tools/rootfs
bootcmd_net=run bootargs_nfs; dhcp; bootm
bootargs=console=ttyAM0, 115200n8
bootcmd=run bootcmd_net
bootdelay=5
baudrate=115200
serverip=192.168.0.106
ipaddr=192.168.0.111
netmask=255.255.255.0
bootfile=uImage
loadaddr=0x42000000
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot} gpmi
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2009.08 (Aug 13 2012 - 16:06:38)

--------------------------------------------------------------------

For your infomation, I am using  Xshell in window xp host.  


Thanks for your support

regards

Jack

ラベル(1)
0 件の賞賛
返信
0 返答(返信)