Serial logs are visible in display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial logs are visible in display

ソリューションへジャンプ
2,168件の閲覧回数
Hrithik
Contributor III

Hi NXP Team,

We are using iMX8MM on Android 11 OS and it uses LVDS bridge based on i2c for display.
While the device boots up, the serial logs(UART logs) get displayed on the display screen.

Attaching picture for reference:

Hrithik_0-1672642135132.jpeg

This is an undesired behaviour and we want to remove this.

Kindly guide us in removing the same.

Thanks

 

0 件の賞賛
返信
1 解決策
2,124件の閲覧回数
Hrithik
Contributor III

Hi @Sanket_Parekh ,

Thanks for the response.
Actually, we figured out that the logs were coming from Kernel as we hadnt defined console and stdout-path in kernel dts files as done in uboot.

Configuring the same in kernel solved the issue.

Regards,
Hrithik

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,125件の閲覧回数
Hrithik
Contributor III

Hi @Sanket_Parekh ,

Thanks for the response.
Actually, we figured out that the logs were coming from Kernel as we hadnt defined console and stdout-path in kernel dts files as done in uboot.

Configuring the same in kernel solved the issue.

Regards,
Hrithik

0 件の賞賛
返信
2,118件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Hrithik 

Issue is resolved. Can I mark this case to close state?

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信
2,105件の閲覧回数
Hrithik
Contributor III
Hi @Sanket_Parekh

Yes, you can close this case.

Thanks,
Hrithik
0 件の賞賛
返信
2,126件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Hrithik ,

I hope you are doing well.
 
Please make sure that you defined the console in defargs environment variable in uboot.
 
Please provide me with the output of printenv in u-boot if this doesn't resolve the issue.
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信