Serial Download Protocol (SDP) security

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Serial Download Protocol (SDP) security

跳至解决方案
2,053 次查看
ceggers
Contributor V

IMX6ULL.pdf states on page 314 (Device Configuration Data, Write data command):

If any of the target addresses do not lie within the allowed
region, none of the values are written. The list of allowable
blocks and target addresses for the chip are provided below.

ceggers_0-1632120703192.png

Page 322 describes the SDP protocol. My expectation is, that the "address white list" for the DCD commands must also apply for the SDP commands. But I didn't find this on the documentation.

Q: Is it save to leave the SDP protocol enabled on a secure device (assuming a HAB version where ERR01087 has been fixed)?

 

0 项奖励
回复
1 解答
2,046 次查看
Yuri
NXP Employee
NXP Employee

@ceggers 
Hello,

  Yes,  it is safe to leave the SDP protocol enabled on a secure device,
assuming ERR01087is fixed.

Regards,
Yuri.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,047 次查看
Yuri
NXP Employee
NXP Employee

@ceggers 
Hello,

  Yes,  it is safe to leave the SDP protocol enabled on a secure device,
assuming ERR01087is fixed.

Regards,
Yuri.

0 项奖励
回复