Selecting i.MX8 EVK 64-bit ARM host platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Selecting i.MX8 EVK 64-bit ARM host platform

677件の閲覧回数
pandivijayaraj
Contributor I

We are looking for i.MX8 EVK for 64-bit ARM host evaluation purpose.
Have compared i.MX 8MQuad EVK, i.MX 8MMini EVK boards available in market.
Both of these boards don't have a full-size SDIO slot available to interface external WiFi device.
Could you suggest a specific i.MX8 EVK with a standard full-size SDIO card available for user.
Thanks.

タグ(2)
0 件の賞賛
返信
1 返信

627件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Pandi Vijayaraj,

As you mentioned, most i.MX8 boards on the market, both NXP’s and from third-parties use micro SD cards and do not come with a full size SD card slot. All boards I’ve seen from Boundary Device, iWave, Variscite and Toradex use the microSD alternative.

The only exception I’ve seen so far would be Phytec. Their phyCORE-i.MX 8M is listed as having a regular SDIO port. I would recommend double checking with them which board or carrier boards have this feature just to be sure before ordering.

https://www.phytec.in/product/system-on-modules/phycore-imx-8m/

My apologies for the inconvenience.

Regards,

0 件の賞賛
返信