Selecting Correct Ram for IMX8M Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Selecting Correct Ram for IMX8M Mini

1,524 Views
wdunkley
Contributor III

I've noticed that the schematics for the IMX8M Mini show 2 GB of ram, while the part numbers supplied are for 16 GB. 

MT53D512M32D2DS-053 WT:D and MT40A512M16LY-075:E should they not be stated at 16GB? Also, can the DDR version run with only one of the dies of ram(if they really are 8GB each) and does it matter which die is placed? Also I'm having the hardest time getting ahold of data sheet for any of the ram. Micron doesn't seem to want to give it up easily and since I don't have Orcad and Altium says it can't import the development files I'm stuck making the footprints.

Labels (1)
0 Kudos
Reply
2 Replies

1,443 Views
b36401
NXP Employee
NXP Employee

Please note that MT53D512M32D2DS-053 is 16Gb part. "Gb" means gigabits not gigabytes. It is exactly 2 gigabytes.
And MT40A512M16LY-075:E is 8Gb part, it is 1 gigabyte.

0 Kudos
Reply

1,443 Views
wdunkley
Contributor III

After all those years of correcting people about how fast their internet really was, it finally got turned around and shoved in my face. HA, Thank You Victor

0 Kudos
Reply