Security configuration on www.nxp.com server throws unexpected SSL3_GET_RECORD error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Security configuration on www.nxp.com server throws unexpected SSL3_GET_RECORD error

921件の閲覧回数
arturobuzarra
Contributor III

I obtain this SSL3_GET_RECORD error from time to time but many times it makes impossible build a yocto recipe when it is necessary an external binary downloaded from www.nxp.com server:

This is the error from bitbake console:

HOME="/home/builder"; /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-dpu-g2d-1.7.0.bin' --progress=dot -v failed with exit code 4, output:

--2019-07-24 07:52:35--  https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-dpu-g2d-1.7.0.bin

Resolving www.nxp.com (www.nxp.com)... 104.109.74.227 Connecting to www.nxp.com (www.nxp.com)|104.109.74.227|:443... connected.

HTTP request sent, awaiting response... 200 OK

Length: 2128718 (2.0M) [application/octet-stream] Saving to: ‘<http://buildserver:8080/job/thud/ws/projects/downloads/imx-dpu-g2d-1.7.0.bin%E2%80%99>

 

     0K .......... .......... .......... .......... ..........  2%  701K 3s

    50K .......... .......... .......... .......... ..........  4%  929K 2s

   100K .......... .......... .......... .......... ..........  7% 4.40M 2s

   150K .......... .......... .......... .......... ..........  9% 1.28M 2s

   200K .......... .......... .......... .......... .......... 12% 4.21M 1s

   250K .......... .......... .......... .......... .......... 14% 6.42M 1s

   300K .......... .......... .......... .......... .......... 16% 1.74M 1s

   350K .......... .......... .......... .......... .......... 19% 8.81M 1s

   400K .......... .......... .......... .......... .......... 21% 6.87M 1s

   450K .......... .......... .......... .......... .......... 24% 11.0M 1s

   500K .......... .......... .......... .......... .......... 26% 8.68M 1s

   550K .......... .......... .......... .......... .......... 28% 10.0M 1s

   600K .......... .......... .......... .......... .......... 31% 14.1M 1s

   650K .......... .......... .......... .......... .......... 33% 2.52M 1s

   700K .......... .......... .......... .......... .......... 36% 9.41M 0s

   750K .......... .......... .......... .......... .......... 38% 9.95M 0s

   800K .......... .......... .......... .......... .......... 40% 10.1M 0s

   850K .......... .......... .......... .......... .......... 43% 14.1M 0s

   900K .......... .......... .......... .......... .......... 45% 9.56M 0s

   950K .......... .......... .......... .......... .......... 48% 12.3M 0s

  1000K .......... .......... .......... .......... .......... 50% 10.5M 0s

  1050K .......... .......... .......... ....                  52% 2.91M=0.3s

 

2019-07-24 07:52:36 (3.35 MB/s) - Read error at byte 1110814/2128718 (error:1408F119:SSL routines:SSL3_GET_RECORD:decryption failed or bad record mac). Retrying.

 

--2019-07-24 07:52:37--  (try: 2)  https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-dpu-g2d-1.7.0.bin

Connecting to www.nxp.com (www.nxp.com)|104.109.74.227|:443... connected.

HTTP request sent, awaiting response... 206 Partial Content

Length: 2128718 (2.0M), 1017904 (994K) remaining [application/octet-stream] Saving to: ‘<http://buildserver:8080/job/thud/ws/projects/downloads/imx-dpu-g2d-1.7.0.bin%E2%80%99>

 

        [ skipping 1050K ]

  1050K ,,,,,,,,,, ,,,,,,,,,, ,,,,,,,,,, ,,,,...... .......... 52% 31.2M 0s

  1100K .......... .......... .......... .......... .......... 55%  548K 1s

  1150K .......... .......... .......... .......... .......... 57% 2.97M 1s

  1200K .......... .......... .......... .......... .......... 60% 1.71M 1s

  1250K .                                                      60% 3245G=0.1s

 

2019-07-24 07:52:38 (1.18 MB/s) - Read error at byte 1281742/2128718 (error:1408F119:SSL routines:SSL3_GET_RECORD:decryption failed or bad record mac). Giving up.

 

 

ERROR: imx-dpu-g2d-1.7.0-r0 do_fetch: Fetcher failure for URL: 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-dpu-g2d-1.7.0.bin;fsl-eula=true'. Unable to fetch URL from any source.

ERROR: imx-dpu-g2d-1.7.0-r0 do_fetch: Function failed: base_do_fetch

NOTE: recipe imx-dpu-g2d-1.7.0-r0: task do_fetch: Failed

After debugging the issue, and building the same recipe from different regions, if the resolved IP for the host www.nxp.com is 104.109.74.227, the wget command fails with the SSL error:

Read error at byte 1110814/2128718 (error:1408F119:SSL routines:SSL3_GET_RECORD:decryption failed or bad record mac). Retrying.

but if I modify my /etc/hosts to resolve www.nxp.com with the IP 23.65.6.72 (which I obtain from a different region) it starts working fine.

I think it is a different security configuration between the mirrors of www.nxp.com,

Could you confirm it?

Thanks,

0 件の賞賛
返信
1 返信

831件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello  Arturo Buzarra,

Thank you for reporting this issue. There are many servers used and it could be possible that one of these was having problems. Some tests were run using IP 104.109.74.227 but the problem was not reproduced.

Would it be possible to test again to see if this issue persists or if it was a temporary problem? If it is still present, please let us know the exact time the issue was encountered. If you are working on different hosts, are all seeing the same problems?

Regards,

0 件の賞賛
返信