Security Reference Manual for i.MX 6QP/DP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Security Reference Manual for i.MX 6QP/DP

跳至解决方案
2,290 次查看
takayuki_ishii
Contributor V

Hello

Our customer hope to obtain a "Security Reference Manual for i.MX6QuadPlus", 

But it have no link for it on Document page of Web.

Do you have a plan to release new document for iMX6DP/QP?

Or can it use for iMX6Dual/Quad's one?

Best regards,

Ishii.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,478 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi takayuki,

Yes the customer can use the 6DQ SRM, as we do not have a dedicated one for 6DQPlus

 

SRM: http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

 

The customer also needs to look at EB810 as there are a couple of fusing updates. Section 6 covers security.

 

EB810 app note: http://cache.nxp.com/assets/documents/data/en/engineering-bulletins/EB810.pdf

 

Also you can see there are no HAB difference between these devices:

 

HAB Versions and Differences in NXP MPU & MCU processors 

 

The only other modifications would be the Central Security Unit (CSU) peripheral mapping since we do have some additional modules on 6DQPlus.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,479 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi takayuki,

Yes the customer can use the 6DQ SRM, as we do not have a dedicated one for 6DQPlus

 

SRM: http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

 

The customer also needs to look at EB810 as there are a couple of fusing updates. Section 6 covers security.

 

EB810 app note: http://cache.nxp.com/assets/documents/data/en/engineering-bulletins/EB810.pdf

 

Also you can see there are no HAB difference between these devices:

 

HAB Versions and Differences in NXP MPU & MCU processors 

 

The only other modifications would be the Central Security Unit (CSU) peripheral mapping since we do have some additional modules on 6DQPlus.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复