Security Reference Manual for i.MX 6QP/DP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Security Reference Manual for i.MX 6QP/DP

Jump to solution
2,316 Views
takayuki_ishii
Contributor V

Hello

Our customer hope to obtain a "Security Reference Manual for i.MX6QuadPlus", 

But it have no link for it on Document page of Web.

Do you have a plan to release new document for iMX6DP/QP?

Or can it use for iMX6Dual/Quad's one?

Best regards,

Ishii.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,504 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi takayuki,

Yes the customer can use the 6DQ SRM, as we do not have a dedicated one for 6DQPlus

 

SRM: http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

 

The customer also needs to look at EB810 as there are a couple of fusing updates. Section 6 covers security.

 

EB810 app note: http://cache.nxp.com/assets/documents/data/en/engineering-bulletins/EB810.pdf

 

Also you can see there are no HAB difference between these devices:

 

HAB Versions and Differences in NXP MPU & MCU processors 

 

The only other modifications would be the Central Security Unit (CSU) peripheral mapping since we do have some additional modules on 6DQPlus.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,505 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi takayuki,

Yes the customer can use the 6DQ SRM, as we do not have a dedicated one for 6DQPlus

 

SRM: http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

 

The customer also needs to look at EB810 as there are a couple of fusing updates. Section 6 covers security.

 

EB810 app note: http://cache.nxp.com/assets/documents/data/en/engineering-bulletins/EB810.pdf

 

Also you can see there are no HAB difference between these devices:

 

HAB Versions and Differences in NXP MPU & MCU processors 

 

The only other modifications would be the Central Security Unit (CSU) peripheral mapping since we do have some additional modules on 6DQPlus.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply