Securing JTAG on i.mx28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Securing JTAG on i.mx28

737 Views
abhijithsoman
Contributor I

I'm using i.mx283 (i.MX283 Processors|High-Performance|NXP )

Couldn't find any documents on how to disable/partially disable JTAG port. 

https://www.nxp.com/docs/en/application-note/AN4686.pdf  Is this application note valid for i.mx28?  

Is it possible to disable JTAG memory access(keeping boundary scan enabled) ?

Is it possible to do this without any manufacturing tools, directly from the Linux running on the processor?

Thanks,

- Abhijith

Labels (2)
0 Kudos
2 Replies

507 Views
abhijithsoman
Contributor I

Hi Igor,

Thank you for the answer.

Could you explain, how can I burn the fuse bit from Linux?

-Abhijith

0 Kudos

507 Views
igorpadykov
NXP Employee
NXP Employee

Hi Abhijith

yes this is possible burning bit0 fuse on address  HW_OCOTP_CUSTCAP described in

sect. 20.4.18 Customer Capability Shadow Register (HW_OCOTP_CUSTCAP) i.MX28 Reference Manual

https://www.nxp.com/docs/en/reference-manual/MCIMX28RM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos