SecureBoot with mfg_tools issues with signature.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SecureBoot with mfg_tools issues with signature.

1,126 次查看
pracette
Contributor I

Hello,

I've been following the guide AN4581, but I'm still getting issues when uploading my signed u-boot.

We are using a imx6 duallite on a custom board.

Here are the output of the commands to know the addresses and offsets:

od -X -N 0x20 {file}
0000000 402000d1 17800000 00000000 177ff42c
0000020 177ff420 177ff400 17875000 00000000
0000040

od -x -j 0x2c -N 4 --endian=big {file}
0000054 d202 f040
0000060

Hab status is reporting : 

--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x24 0x41 0x33 0x18 0xc0 0x00
0xca 0x00 0x1c 0x00 0x02 0xc5 0x00 0x00
0x00 0x00 0x0d 0x44 0x17 0x7f 0xf4 0x00
0x00 0x07 0x5c 0x00 0x00 0x91 0x00 0x00
0x00 0x00 0x02 0xf8

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_SIGNATURE (0x18)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)

Attached you will find my my signing scripts, my csf file as well as the full output from hab_status.

I have a feeling the offset in mod_4_mfgtool is wrong but I don't know where to get it from.

Thanks for you help

Patrick

标签 (1)
0 项奖励
回复
1 回复

986 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Patrick

one can check

https://community.nxp.com/message/600808 

for getting help with security software may be recommended to proceed with NXP Professional Services

NXP Professional Services|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复