I use HAB successfully authenticates the signed image .HAB didn't generate any events.I use fuse prog 1 3 0x2000000 this commond to close the devices.I can load u-boot images that have been signed.But when I load u-boot images that don't have been signed.The devices cann't power on . I can't get any message from the USB port and Serial port.They can't work.What should I do to save my devices.And what's the reason that my devices can't power on.
解決済! 解決策の投稿を見る。
Hi longlong
please check AN4581 Secure Boot on i.MX50, i.MX53, i.MX6 and i.MX7 Series using HABv4
https://www.nxp.com/docs/en/application-note/AN4581.pdf
Note, once burned, fuse can not be restored to original state.
Best regards
igor
Hi,
This is normal - once you have closed the device, the secure boot feature will not let anymore the execution passing to u-boot if the signature checking will fail. So, you'll be able to run only u-boot/images signed with the proper keys in sync with the SRK hashes.
Regards,
Marius
I have closed my device and secured my device ,hab_status shows that Secure boot enabled.I have downloaded a signed u-boot.imx ,but why I can download a no signed boot.img .It's not secure.I think a signed u-boot.imx can't load a no signed boot.img.Can you help me.Thank you!