Secure Boot issue on imx6ull

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure Boot issue on imx6ull

5,535件の閲覧回数
kwroot
Contributor I

Hi! I'm trying to implement secure boot on imx6ull (Yocto - sumo release). Using the related guide at this link, no error shows up. In fact, after burning the public keys on efuses the hab_status resulted always ok even in the next boot (Secure boot disabled HAB Configuration: 0xf0, HAB State: 0x66 No HAB Events Found!). Considering that no HAB Events were found, i've burnt the last fuse (fuse prog 0 6 0x2), but now i'm not able to boot the system.

The error is the following:

---

## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000

Authenticate image from DDR location 0x82000000...
Check CSF for Write Data command before authenticating image
Error - CSF lies outside the image bounds
Authenticate zImage Fail, Please check

-----

And the hab_status still not shows HAB events.

How can i solve this problem?

Thank you in advance!

 

0 件の賞賛
返信
9 返答(返信)

2,883件の閲覧回数
ljm3721
Contributor I

Hi kwroot:
Thank you for sharing. I am also working on secure boot on the imx6ull board. I want to know if you have successfully solved this problem later. I hope you can provide information to help me solve this problem.

0 件の賞賛
返信

5,325件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

5,319件の閲覧回数
kwroot
Contributor I

Hi Igor,

I followed the HAB tutorial step by step. The Paragraph 3.10 says "Make sure there are not events before proceeding to the next step". But even if no HAB event were found, the system now is not booting. This means that i cannot be 100% sure that the HAB is correctly done until burning the SEC_CONFIG[1] fuse bit. Now i'm not confident to make further test on other imx6ull cpu's.

Questions:

  1. Is there some virtual safe-environment for make this kind of test?
  2. The tutorial use the 2.3.3 cfu's version. I've used the cst 3.1.0. Could this be a problem?

Thank you for your support.

Best

0 件の賞賛
返信

5,230件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kwroot

 

>Is there some virtual safe-environment for make this kind of test?

no

>The tutorial use the 2.3.3 cfu's version. I've used the cst 3.1.0. Could this be a problem?


cst 3.1.0 is latest version, it should not cause problem.

 

Best regards
igor

0 件の賞賛
返信

5,198件の閲覧回数
kwroot
Contributor I

Hi Igor,

I've seen all the posts  concerning the "CSF lies outside the image bounds" error, but i'm still stucked. I also checked step by step all the HAB instruction, and all seems correctly done. Could the problem be indexing related even if the unlocked system correctly boot with no HAB events?

You can find all the .csf below:

------ var-default.csf ------ 

[Header]
Version = 4.1
Hash Algorithm = sha256
Engine = ANY
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Address Offset Length Data File Path

 

----- u-boot-ivt.img.csf ------

[Header]
Version = 4.1
Hash Algorithm = sha256
Engine = SW
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Address Offset Length Data File Path
Blocks = 0x85ffffc0 0x0000 0x00057020 "u-boot-ivt.img"

 

------ SPL.csf -------

[Header]
Version = 4.1
Hash Algorithm = sha256
Engine = SW
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Address Offset Length Data File Path
Blocks = 0x00908400 0x00000000 0x0000ac00 "SPL"

[Unlock]
Engine = CAAM
Features = RNG

 

------ zImage-ivt.csf -------

[Header]
Version = 4.1
Hash Algorithm = sha256
Engine = SW
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Address Offset Length Data File Path
Blocks = 0x82000000 0x0000 0x6a3020 "zImage-ivt"

 

---------------

Can you give me an hint?

Thank you for the support.

Best

 

0 件の賞賛
返信

5,184件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kwroot

 

what bsp used in the case, could you try from  source.codeaurora.org/external/imx/linux-imx repository

https://source.codeaurora.org/external/imx/uboot-imx/tree/?h=imx_v2020.04_5.4.24_2.1.0
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.24_2.1.0

Rebuild all from scratch following guidelines from:

https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4?h=imx_v2020.04_5.4.24_2.1.0

 

Best regards
igor

0 件の賞賛
返信

5,176件の閲覧回数
kwroot
Contributor I

Hi Igor,

I've seen the posts related to the "Error - CSF lies outside the image bounds" issue, but i'm still stacked. I checked all the step of HAB tutorial, and all seems correctly done. Could the problem be indexing related even if the unlocked system correctly boot?

You can find all the file .csf file used below.

------ var-default.csf ------ 

[Header]
Version = 4.1
Hash Algorithm = sha256
Engine = ANY
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Address Offset Length Data File Path

 

------ u-boot-ivt.img.csf ------ 

[Header]
Version = 4.1
Hash Algorithm = sha256
Engine = SW
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Address Offset Length Data File Path
Blocks = 0x85ffffc0 0x0000 0x00057020 "u-boot-ivt.img"

 

------ SPL.csf ------ 

[Header]
Version = 4.1
Hash Algorithm = sha256
Engine = SW
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Address Offset Length Data File Path
Blocks = 0x00908400 0x00000000 0x0000ac00 "SPL"

[Unlock]
Engine = CAAM
Features = RNG

------ zImage-ivt.csf ------ 

[Header]
Version = 4.1
Hash Algorithm = sha256
Engine = SW
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Address Offset Length Data File Path
Blocks = 0x82000000 0x0000 0x6a3020 "zImage-ivt"

 

Can you give me some further hint?

Thank you for the support,

Best

 

0 件の賞賛
返信

5,240件の閲覧回数
kwroot
Contributor I

Dear Igor,

I look forward to your reply.

Thank you in advance!

0 件の賞賛
返信

5,499件の閲覧回数
kwroot
Contributor I

EDIT:

If i try to reflash with the same sd card i get this error:

-------

Authenticate image from DDR location 0x82000000...
Check CSF for Write Data command before authenticating image

Secure boot enabled

HAB Configuration: 0xcc, HAB State: 0x99

--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0f 0xc0 0x00
0xbe 0x00 0x0c 0x00 0x03 0x17 0x00 0x00
0x00 0x00 0x00 0x48

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_INDEX (0x0F)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)

Authenticate zImage Fail, Please check

0 件の賞賛
返信