Secure Boot i.MX 6 & HAB 4.1.2

cancel
Showing results for 
Search instead for 
Did you mean: 

Secure Boot i.MX 6 & HAB 4.1.2

Jump to solution
587 Views
mklug_xx
Contributor I

Document AN4581, Secure Boot on i.MX50, i.MX53, and i.MX 6 Series using HABv4, mentions Fast Authentification in Appendix B.

My question is, is there a series of i.MX 6 processors, which have HAB 4.1.2 on board?

-Mike

0 Kudos
1 Solution
347 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michael

hab versions are described on p.15 presentation

ftf-ins-f1208.pdf | NXP Community

HAB 4.1.2 is used on i.MX6SX and MX7D, MX6UL  4.2.2

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
348 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michael

hab versions are described on p.15 presentation

ftf-ins-f1208.pdf | NXP Community

HAB 4.1.2 is used on i.MX6SX and MX7D, MX6UL  4.2.2

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------