Second UART on i.MX8MQ-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Second UART on i.MX8MQ-EVK

Jump to solution
291 Views
lcothales
Contributor I

Hi,

I tried to use the second UART of my iMX8MQ-EVK to print the output of the Linux console.
I built a Linux with yocto (version : imx-6.1.36-2.1.0).
I have enabled all uarts in the device tree. So, in my Linux, I have ttymxc0/1/2/3 but
none sends traces to my minicom on ttyUSB1 when I change console boot parameter via u-boot.

The second UART is dedicated to M4 or it can be used with A53 ?
Is there a way to enable the second UART ?

Thanks in advance,

0 Kudos
Reply
1 Solution
281 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

As this post suggests, you need to make changes starting from atf, could you follow the guide and feed if you succeed?

Regards

View solution in original post

0 Kudos
Reply
1 Reply
282 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

As this post suggests, you need to make changes starting from atf, could you follow the guide and feed if you succeed?

Regards

0 Kudos
Reply