Second RGB output possible for i.MX6D/Q?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Second RGB output possible for i.MX6D/Q?

ソリューションへジャンプ
1,501件の閲覧回数
kirgene
Contributor II

Hello,

I'm developing custom board based on i.MX6D.

In datasheet "i.MX 6Dual/6Quad Applications Processors for Consumer Products" section "4.11.10.4 IPU Display Interface Signal Mapping" says each IPU has its own LCD RGB interface. As I understand some of pins for second RGB interface (DISP1) are shared with other components and they need to be configured to use as DISP1.

The question is can I use DISP1 and DISP0 in parallel for displaying different FullHD content on two monitors at the same time.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,377件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Yevhen

yes both DISP1 and DISP0 can be used in parallel

for displaying different content on two monitors at the same time,

one needs to set correctly iomux settings for these signals.

1.jpg

2.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,378件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Yevhen

yes both DISP1 and DISP0 can be used in parallel

for displaying different content on two monitors at the same time,

one needs to set correctly iomux settings for these signals.

1.jpg

2.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,377件の閲覧回数
kirgene
Contributor II

Thanks!

I have two additional questions on this subject:

1) Is it possible to have 5 display interfaces working at the same time displaying different content:

HDMI

LVDS (2x)

RGB (2x)

On the other hand i.MX6 datasheet claims that processor support 4 simultaneously working displays at the same time.

What are the real capabilities?

2) And what software configuration should be done to enable second RGB interface?

0 件の賞賛
返信