Scope of notes in register_programming_aid for the i.MX6 DDR Stress Test Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Scope of notes in register_programming_aid for the i.MX6 DDR Stress Test Tool

ソリューションへジャンプ
1,208件の閲覧回数
torus1000
Contributor V

Hi,

I'm checking DDR memory timings of my i.MX6Q board now.
I would like to change REF_SEL to choose 64kHz in terms of testing half refresh cycle of DDR3 memory.
Then I found a Note for REFR bit in MDREF register which described as following.


      MX6Q_SabreSD_DDR3_register_programming_aid_v2.3.xlsx
      https://community.nxp.com/docs/DOC-105963

      See $F$125;

"MDREF register setting. Note, only parameter REFR is programmable, all other parameters are fixed as follows:
REF_CNT: 0x0 (default value, parameter not used)
REF_SEL: 0x1 (choose 32KHz clock to trigger refresh cycle)
START_REF: Manually start refresh cycle, set to 0 for normal operations"

I'm confusing there is no such description in ref manual; REF_SEL is fixed.

(Q)  Scope of this Notes are just for the calibration purpose, right?
       (Can I ignore this Note when I test another DDR refresh rate?)

Can anyone help me?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,139件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

>(Q)  Scope of this Notes are just for the calibration purpose, right?

right

>       (Can I ignore this Note when I test another DDR refresh rate?)

yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,140件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

>(Q)  Scope of this Notes are just for the calibration purpose, right?

right

>       (Can I ignore this Note when I test another DDR refresh rate?)

yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信