Hi,
I'm checking DDR memory timings of my i.MX6Q board now.
I would like to change REF_SEL to choose 64kHz in terms of testing half refresh cycle of DDR3 memory.
Then I found a Note for REFR bit in MDREF register which described as following.
MX6Q_SabreSD_DDR3_register_programming_aid_v2.3.xlsx
https://community.nxp.com/docs/DOC-105963
See $F$125;
"MDREF register setting. Note, only parameter REFR is programmable, all other parameters are fixed as follows:
REF_CNT: 0x0 (default value, parameter not used)
REF_SEL: 0x1 (choose 32KHz clock to trigger refresh cycle)
START_REF: Manually start refresh cycle, set to 0 for normal operations"
I'm confusing there is no such description in ref manual; REF_SEL is fixed.
(Q) Scope of this Notes are just for the calibration purpose, right?
(Can I ignore this Note when I test another DDR refresh rate?)
Can anyone help me?
已解决! 转到解答。
Hi torus1000
>(Q) Scope of this Notes are just for the calibration purpose, right?
right
> (Can I ignore this Note when I test another DDR refresh rate?)
yes
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi torus1000
>(Q) Scope of this Notes are just for the calibration purpose, right?
right
> (Can I ignore this Note when I test another DDR refresh rate?)
yes
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------