Saving power consumption with Ethernet communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Saving power consumption with Ethernet communication

698 Views
yuji_fuseki
Contributor II

Hi,

 

Our product design is started with IMX6DL.

Now, I have a requirement that

"power consumption of our product is less than 2W while waiting for Power-On command from external controller during standby mode"

To satisfy this requirement, do we have any method to save IMX6DL power consumption as long as possible? 

 <Example>

 IMX6 works with low clock mode, or providing power supply voltage to only related IF, such as NVCC_RMII

And, please refer below diagram for your understanding.

pastedImage_3.png

Best regards,

Yuji

Tags (2)
0 Kudos
3 Replies

674 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuji

I am afraid power consumtion data for such use case is not available.

Available power consumption data can be found in AN4576, please pay

attention to sect.4 Reducing power consumption

i.MX 6DualLite Power Consumption Measurement

>IMX6 works with low clock mode, or providing power supply voltage to only related IF, such as NVCC_RMII

for i.MX6DL all power supplies should be on even for unused modules.

For requirement "power consumption of our product is less than 2W" may be recommended to

apply to Professional Services Software Technologies Form | NXP Semiconductors 

as many customers achieved necessary power numbers making various software optimizations

using this service.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

671 Views
yuji_fuseki
Contributor II

Hi, Igor

Thanks for your reply.
If we realize to reduce power consumption by entering low power mode, some of mode still can use RMII function?

>IMX6 works with low clock mode, or providing power supply voltage to only related IF, such as NVCC_RMII
>
for i.MX6DL all power supplies should be on even for unused modules.
Is this regardless of power mode?

 

0 Kudos

659 Views
yuji_fuseki
Contributor II

Hi,
Please help to answer for my question.

 

0 Kudos