Sample source code for operation which i.MX7ULP is in to VLLS mode by M4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sample source code for operation which i.MX7ULP is in to VLLS mode by M4

1,107 次查看
ko-hey
Senior Contributor II

Hi everyone,

 

I'm finding a sample code for operation which i.MX7ULP is in to VLLS mode by M4.

Since the A7 side has the Linux source, I can understand the processing flow somehow, but is it OK for the M4 side to have the same flow ?

 

Could you tell me the place of source code if someone know ?

 

Ko-hey

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,087 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

sample code can be found in M4 SDK_MX7ULP EVK power_mode_switch example

available on

Welcome | MCUXpresso SDK Builder 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复