Sample source code for operation which i.MX7ULP is in to VLLS mode by M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample source code for operation which i.MX7ULP is in to VLLS mode by M4

1,066 Views
ko-hey
Senior Contributor II

Hi everyone,

 

I'm finding a sample code for operation which i.MX7ULP is in to VLLS mode by M4.

Since the A7 side has the Linux source, I can understand the processing flow somehow, but is it OK for the M4 side to have the same flow ?

 

Could you tell me the place of source code if someone know ?

 

Ko-hey

Labels (1)
0 Kudos
Reply
1 Reply

1,046 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

sample code can be found in M4 SDK_MX7ULP EVK power_mode_switch example

available on

Welcome | MCUXpresso SDK Builder 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply