Sample code to use i.MX6DQ EIM burst access.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample code to use i.MX6DQ EIM burst access.

Jump to solution
2,916 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6DQ EIM.

They want to know where is the sample code to use EIM burst read / write.

Is there some sample?

Especially, I will appreciate if you teach me where is the code to use EIM burst write when BL (chapter 22.9..1 in IMX6DQRM Rev.2) = 100 (Continuous burst length).

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
1 Solution
2,195 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am not aware of such examples, however I think one can use attached i.MX53 example

and modify it for i.MX6 using i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,195 Views
bipin7301
Contributor II

Hi @satoshishimoda 

I was also trying to do similar kind of thing but in i.MX7.

 

Were you able to achieve what you were trying to do ?

 

Can you please share your understanding/coding details ?

 

Regards

Bipin Kumar

0 Kudos
Reply
2,196 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am not aware of such examples, however I think one can use attached i.MX53 example

and modify it for i.MX6 using i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply