Safe mode in i.MX6q Software Mux Control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Safe mode in i.MX6q Software Mux Control

998件の閲覧回数
vijaikumar
Contributor III

Hi All,

         If you see OMAP processors from TI, there is a mode called SAFE_MODE other than the modes supported by the particular PAD control register.

As quoted, the safe_mode in OMAP "avoids any risk of electrical contention by configuring the pin as an input with no functional interface mapped to it. The safe mode is used mainly as the default mode for all pins containing no mandatory interface at the release of power-on reset." Is similar kind of functionality available in i.MX processors.

Regards

Vijai Kumar K

ラベル(6)
タグ(3)
0 件の賞賛
返信
1 返信

897件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vijai

there is no similar mode in i.MX6 processors.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信