Safe mode in i.MX6q Software Mux Control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Safe mode in i.MX6q Software Mux Control

497 Views
vijaikumar
Contributor III

Hi All,

         If you see OMAP processors from TI, there is a mode called SAFE_MODE other than the modes supported by the particular PAD control register.

As quoted, the safe_mode in OMAP "avoids any risk of electrical contention by configuring the pin as an input with no functional interface mapped to it. The safe mode is used mainly as the default mode for all pins containing no mandatory interface at the release of power-on reset." Is similar kind of functionality available in i.MX processors.

Regards

Vijai Kumar K

Labels (6)
Tags (3)
0 Kudos
Reply
1 Reply

396 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vijai

there is no similar mode in i.MX6 processors.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply