Sabresd board : No HDMI output in Android JB 4.2.2 recovery mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabresd board : No HDMI output in Android JB 4.2.2 recovery mode

ソリューションへジャンプ
2,669件の閲覧回数
nickyeh
Contributor II


Hi,

I am trying to do android recovery mode in Sabresd board. In my environment, I use HDMI as output display, no LVDS.

Below is my U-boot bootargs:

console=ttymxc0,115200 init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 vmalloc=400M androidboot.console=ttymxc0 no_console_suspend androidboot.hardware=freescale

To enter recovery mode, I do folllowing steps:

1. copy sabresd_6dq-ota-.... .zip to /cache

2. create a file "command" in /cache/recovery, the contents of this file represent the filename of update package, it should look like below:

   "--update_package=/cache/sabresd_6dq-ota-....zip"

3. in CLI, execute "reboot recovery"

4. system reboot and get into recovery mode

In previous android release (imx-android-13.4.1), I can see rolling star in Android icon on HDMI display which represents the update process is running.

But In JB 4.2.2 ga release, No HDMI display, but I can confirms the recovery is running.

I had try to add "--show_text" in command file and it can display static pic, but cannot see like previous "rollong star" in Android icon.

Anyone can figure out what I miss?

Thanks in advanced.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,417件の閲覧回数
nickyeh
Contributor II

Hi,

I got normal HDMI output in recovery mode while boot with below bootargs:

console=ttymxc0,115200 init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=16 vmalloc=400M androidboot.console=ttymxc0 no_console_suspend androidboot.hardware=freescale

The different is "bpp".

Anyway, I can modify u-boot to replace with this argument while system want to get in recovery mode.

Thanks

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,418件の閲覧回数
nickyeh
Contributor II

Hi,

I got normal HDMI output in recovery mode while boot with below bootargs:

console=ttymxc0,115200 init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=16 vmalloc=400M androidboot.console=ttymxc0 no_console_suspend androidboot.hardware=freescale

The different is "bpp".

Anyway, I can modify u-boot to replace with this argument while system want to get in recovery mode.

Thanks

0 件の賞賛
返信
1,417件の閲覧回数
nickyeh
Contributor II

Does anyone can help?

0 件の賞賛
返信
1,417件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Did you get an output in the HDMI in normal mode?

Have you tried with different panels? and changing the frequency?

Regards,

Alejandro

0 件の賞賛
返信
1,417件の閲覧回数
nickyeh
Contributor II

Yes, HDMI output work well in normal mode.

The problem in is JB 4.2.2 recovery mode, not in imx-android-13.4.1.

I am not sure the symptom could be duplicated in LCD panel since that is not required in my project.

I will do more experiment with different bootargs (resolution or something else).

Thanks your suggestion.

0 件の賞賛
返信