Hi to all,
I'm working on Sabre-sd board with 1DX module from Murata(based on broadcom/cypress 4343 chip) running Andorid 8.0.
Wi-Fi is working fine, I'm able to connect to an AP and browse internet but I'm still having problem on bringing up bluetooth.
The board has all the modifications required by the Murata guide.
When I try to enable bluetooth from settings the start-up procedure fails during inizialization of of "controller_module" when issuing HCI opcodes:
the firmware seems to be correctly uploaded to the controller (as you can see in the logcat below) and the serial communication with the chip is started (the host receives response to the firsts HCI opcodes) but the communication stops at the same point (opcode= 0xc6d) . I've tried to increase timeout but without succes.
Could you please provide support to solve the issue?
01-17 09:31:23.911 1499 1515 I bt_core_module: module_start_up Starting module "hci_module"
01-17 09:31:23.911 1499 1515 I bt_hci : hci_module_start_up
01-17 09:31:23.912 1499 1529 I bt_osi_thread: run_thread: thread id 1529, thread name hci_thread started
01-17 09:31:23.912 1499 1515 D bt_hci : hci_module_start_up starting async portion
01-17 09:31:23.912 1499 1529 I bt_hci : hci_initialize
01-17 09:31:23.914 1499 1529 I bt_hci : hci_initialize: IBluetoothHci::getService() returned 0xa6530420 (remote)
01-17 09:31:23.915 278 1477 I android.hardware.bluetooth@1.0-impl: BluetoothHci::initialize()
01-17 09:31:23.916 278 1477 I bt_vendor: init
01-17 09:31:23.916 278 1477 I bt_vnd_conf: Attempt to load conf from /etc/bluetooth/bt_vendor.conf
01-17 09:31:23.916 278 1477 D android.hardware.bluetooth@1.0-impl: Open vendor library loaded
01-17 09:31:23.922 278 1477 W bt_vendor: NOTE: BT_VND_PWR_ON now forces power-off first
01-17 09:31:24.445 278 1477 I bt_userial_vendor: userial vendor open: opening /dev/ttymxc4
01-17 09:31:24.450 278 1477 I bt_userial_vendor: device fd = 6 open
01-17 09:31:24.490 278 1531 I bt_hwcfg: bt vendor lib: set UART baud 3000000
01-17 09:31:24.491 278 1531 D bt_hwcfg: Chipset BCM43430A1
01-17 09:31:24.491 278 1531 D bt_hwcfg: Target name = [BCM43430A1]
01-17 09:31:24.491 278 1531 I bt_hwcfg: FW patchfile: /vendor/firmware/bcm/Type_ZP.hcd
01-17 09:31:24.612 278 1531 I bt_hwcfg: bt vendor lib: set UART baud 115200
01-17 09:31:24.613 278 1531 D bt_hwcfg: Settlement delay -- 900 ms
01-17 09:31:24.613 278 1531 I bt_hwcfg: Setting fw settlement delay to 900
01-17 09:31:25.525 278 1531 I bt_hwcfg: bt vendor lib: set UART baud 3000000
01-17 09:31:25.525 278 1531 I bt_hwcfg: Setting local bd addr to 22:22:67:C6:69:73
01-17 09:31:25.526 278 1531 I bt_hwcfg: vendor lib fwcfg completed
01-17 09:31:25.526 278 1531 D android.hardware.bluetooth@1.0-impl: OnFirmwareConfigured result: 0
01-17 09:31:25.526 278 1531 I android.hardware.bluetooth@1.0-impl: Firmware configured in 1.076s
01-17 09:31:25.526 1499 1529 I bt_hci : event_finish_startup
01-17 09:31:25.526 278 1531 I android.hardware.bluetooth@1.0-impl: OnFirmwareConfigured: lpm_timeout_ms 1500
01-17 09:31:25.527 278 1531 D android.hardware.bluetooth@1.0-impl: OnFirmwareConfigured Calling StartLowPowerWatchdog()
01-17 09:31:25.527 1499 1515 I bt_core_module: module_start_up Started module "hci_module"
01-17 09:31:25.527 1499 1532 I bt_osi_thread: run_thread: thread id 1532, thread name bt_workqueue started
01-17 09:31:25.527 1499 1532 I : [0117/093125:INFO:btu_task.cc(108)] Bluetooth chip preload is complete
01-17 09:31:25.528 278 1531 D android.hardware.bluetooth@1.0-impl: low_power_mode_cb result: 0
01-17 09:31:25.528 1499 1532 E bt_att : gatt_profile_db_init: gatt_if=1
01-17 09:31:25.529 1499 1533 I bt_osi_thread: run_thread: thread id 1533, thread name btu message loop started
01-17 09:31:25.530 1499 1534 I bt_osi_thread: run_thread: thread id 1534, thread name module_wrapper started
01-17 09:31:25.530 1499 1534 I bt_core_module: module_start_up Starting module "controller_module"
01-17 09:31:25.530 1499 1534 I bt_controller: start_up ENTER
01-17 09:31:25.530 1499 1529 D bt_hci : event_command_ready sending command opcode= 0xc03
01-17 09:31:25.534 1499 1530 I bt_hci : filter_incoming_event : (HCI_COMMAND_COMPLETE_EVT) got opcode = 0x0c03
01-17 09:31:25.534 1499 1534 I bt_controller: start_up reset done
01-17 09:31:25.534 1499 1529 D bt_hci : event_command_ready sending command opcode= 0x1005
01-17 09:31:25.535 1499 1530 I bt_hci : filter_incoming_event : (HCI_COMMAND_COMPLETE_EVT) got opcode = 0x1005
01-17 09:31:25.535 1499 1534 I bt_controller: start_up buffer request done
01-17 09:31:25.535 1499 1529 D bt_hci : event_command_ready sending command opcode= 0xc33
01-17 09:31:25.536 1499 1530 I bt_hci : filter_incoming_event : (HCI_COMMAND_COMPLETE_EVT) got opcode = 0x0c33
01-17 09:31:25.536 1499 1534 I bt_controller: start_up buffer set done
01-17 09:31:25.536 1499 1529 D bt_hci : event_command_ready sending command opcode= 0x1001
01-17 09:31:25.537 1499 1530 I bt_hci : filter_incoming_event : (HCI_COMMAND_COMPLETE_EVT) got opcode = 0x1001
01-17 09:31:25.537 1499 1534 I bt_controller: start_up read local version done
01-17 09:31:25.537 1499 1529 D bt_hci : event_command_ready sending command opcode= 0x1009
01-17 09:31:25.539 1499 1530 I bt_hci : filter_incoming_event : (HCI_COMMAND_COMPLETE_EVT) got opcode = 0x1009
01-17 09:31:25.539 1499 1534 I bt_controller: start_up read bt address done
01-17 09:31:25.539 1499 1529 D bt_hci : event_command_ready sending command opcode= 0x1002
01-17 09:31:25.540 1499 1530 I bt_hci : filter_incoming_event : (HCI_COMMAND_COMPLETE_EVT) got opcode = 0x1002
01-17 09:31:25.540 1499 1534 I bt_controller: start_up supported commands request done
01-17 09:31:25.540 1499 1529 D bt_hci : event_command_ready sending command opcode= 0x1004
01-17 09:31:25.541 1499 1530 I bt_hci : filter_incoming_event : (HCI_COMMAND_COMPLETE_EVT) got opcode = 0x1004
01-17 09:31:25.541 1499 1534 I bt_controller: start_up read page 0 done
01-17 09:31:25.541 1499 1529 D bt_hci : event_command_ready sending command opcode= 0xc56
01-17 09:31:25.601 1499 1530 I bt_hci : filter_incoming_event : (HCI_COMMAND_COMPLETE_EVT) got opcode = 0x0c56
01-17 09:31:25.602 1499 1534 I bt_controller: start_up simple pairing done
01-17 09:31:25.602 1499 1534 I bt_controller: start_up write host support START
01-17 09:31:25.602 1499 1529 D bt_hci : event_command_ready sending command opcode= 0xc6d
01-17 09:31:25.688 404 420 D ViewRootImpl[bluetooth]: updatePointerIcon called with position out of bounds
01-17 09:31:26.916 281 389 I display : alloc cache buffer err:0
01-17 09:31:30.602 1499 1518 E bt_hci : command_timed_out: 1 commands pending response
01-17 09:31:30.602 1499 1518 E bt_hci : command_timed_out: Waited 5000 ms for a response to opcode: 0xc6d *matches timer*
01-17 09:31:30.602 1499 1518 E bt_hci : command_timed_out: Size 5 Hex 6d 0c 02 01
01-17 09:31:30.602 1499 1518 E bt_hci : command_timed_out: requesting a firmware dump.
01-17 09:31:30.603 1499 1518 E bt_hci : command_timed_out restarting the Bluetooth process.
01-17 09:31:31.103 1499 1518 F libc : Fatal signal 6 (SIGABRT), code -6 in tid 1518 (alarm_default_c), pid 1499 (droid.bluetooth)