Hi there
I'm trying to orientate myself in Freescale's kernel source and support to Sabrelite (imx6q) with the Vivante support.
What I would like to be able to do is to download the newest kernel supported with imx6q/sabrelite/vivante support and build it myself.
Where is the correct location for acquiring those things ?
I have looked through Freescale · GitHub where there are listed several projects like:
- meta-fsl-arm
- meta-fsl-arm-extra
- fsl-community-bsb-base
.
.
and several more, but I am having a hard time to see what needs to be downloaded in order to have the required material (code) in my hand so I can build it myself.
I have before downloaded some older source from Linaro (3.0) but I would like to have some more recent kernel to build with the Sabrelite support.
Can anyone give my some basic insight into how Freescale is operating this now ?
Kind regards
Einar
 
					
				
		
Hi Yixing
I have managed to complete this task by using the kernel from: boundarydevices/linux-imx6 · GitHub and the vivante binaries are from the gpu SDK here: Index of /buildsources/g/gpu-viv-bin-mx6q
With this I have everything I need for now. I must admit that I am keen on taking the Yocto path but that will be my next step after we have managed to bring our iMX6q based board up. That will happen within the next two months.
Thanks for you help.
Regards
Einar
 
					
				
		
Hi
I basically need to have the correct kernel source and build it myself because we maintain our own debian/ubuntu distro where everything is compiled with Linaro's toolchain.
Could you maybe recommend me on how to work out those patches in order to produce a complete kernel source for me ? where I don't have to build it with bitbake or do any other compilation. I just need to source to be proper.
Thanks for the support
Einar
 
					
				
		
Einar
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel free
to contact Freescale.
Thanks,
Yixing
FabioEstevam Fabio, could you help me answering Einar's below question?
 
					
				
		
 fabio_estevam
		
			fabio_estevam
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		For mx6qsabrelite, the following kernel source is recommended:
boundarydevices/linux-imx6 at boundary-imx_3.0.35_1.1.1 · GitHub
 
					
				
		
So, in order to understand the concept here, then Freescale are providing some board recipes that are patched into some version of the mainline Linux ?
Hi Einar,
You may have figured out what you mentioned is correct.Take a look at this folder: sources/meta-fsl-arm/recipes-kernel/linux and check files linux-imx_3.0.35.bb and linux-imx.inc. There you see the git repo where the fetching is done and the SRCREV hash string (where the git HEAD will be pointing to). This upstream repo has all necessary commits which were created under a mainline (linus) repo.
Leo
have you created an image with bitbake?
Follow the instructions on the README's but you should do something like this
$ source setup-environment imx6qsabrelite
$ bitbake core-image-minimal
The recipe which builds the sabre lite kernel is on ../sources/meta-fsl-arm/recipes-kernel/linux/ and once the (bit)baking ends, the source code is somewhere on tmp/work and the resulted images are on tmp/deploy.
Leo
 
					
				
		
If you want to go the openembedded way, then I'd recommend Yocto. I've used it for building a whole distribution (Poky), including kernel and running it on my sabrelite board. Follow directions here:
i.MX Yocto: how can I build the Freescale Yocto Images?
There is an active community here:https://lists.yoctoproject.org/listinfo/meta-freescale
If you have any questions or patches to submit, please submit them to the meta-freescale list.
From my understanding, Vivante drivers are closed source. There is an attempt to reverse-engineer them here: