Sabrelite i.mx6 ethernet connection (big latency and connection is cut regularly every 30 sec)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabrelite i.mx6 ethernet connection (big latency and connection is cut regularly every 30 sec)

1,400 Views
mohamad-ahmad
Contributor III

hello,

I posted this problem earlier (Big Latencies in the ethernet connection for the I.MX6 sabrelite ) but is not resolved.

I have tried the connection ssh to sabrelite in two ways:

  1. connect the board by ethernet to the existed network and after that use ssh connection.
  2. connect the board with ethernet directly to my computer (dhcp server) and use ssh connection.

In the two ways the same problem.

you can watch this video which shows the ethernet port on my board and the regular disconnecting problem.

sabrelit_ethernet_connection.mp4 - Google Drive 

Can someone help me please,

thank you,

Mohamad

Labels (2)
0 Kudos
Reply
2 Replies

1,222 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mohamad

sabrelite board is supported by its vendor boundary devices, in general

one can try to post on meta-fsl-arm mailing list, so that someone familiar with

that board could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Alternatively one can try bsps from timesys

https://linuxlink.timesys.com/docs/gsg/i.MX6QSABRELite

or use nxp reference boards.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,222 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Mohamad,

Have you try to post your question on the Boundary Devices​ place?  They use a different BSP  based on the NXP, but they change a lot of stuff, maybe you can ask them, they have also a support page : https://boundarydevices.com/support/


Have a great day,

Jaime

0 Kudos
Reply