Sabrelite brick, not able to start up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabrelite brick, not able to start up

6,766件の閲覧回数
chewhouming
Contributor III

i brick my sabrelite, when i tried to burn in bootfromSDcard image using putty.

Now i cannot bootup at all, believe the internal bootloader is fried.

Anyone has any answer.

does this link provide correct answer

Getting Started Guide for iMX6 SabreLite - RidgeRun Developer Connection

11 返答(返信)

5,534件の閲覧回数
EricNelson
Senior Contributor II

Hi Chew,

I think what you're looking for is here:

     http://boundarydevices.com/unbricking


Or if you're using a Windows PC:

     http://boundarydevices.com/windows-users-and-unbricking

0 件の賞賛
返信

5,534件の閲覧回数
chewhou
Contributor II

hi

I been to this page.

i could not see a “Freescale” device show up in lsusb:

0 件の賞賛
返信

5,534件の閲覧回数
EricNelson
Senior Contributor II

Hi Chew,

Please try both 10 and 01 positions of SW1.

0 件の賞賛
返信

5,534件の閲覧回数
chewhouming
Contributor III

I brick my sabrelite yesterday, i can't get any response from sabrelite, and below is what i did

In ucl2.xml, I add 6 lines before the line "List name=Sabre-SD-uBootOnly"

<LIST name="Sabre-SD-uBootOnly" desc="Only boot u-Boot.bin">

    <CMD state="BootStrap" type="boot" body="BootStrap" file ="u-boot.bin" >Loading U-boot</CMD>

    <CMD state="BootStrap" type="load" file="initramfs.cpio.gz.uboot" address="0x10C00000"

        loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Loading Initramfs.</CMD>

    <CMD state="BootStrap" type="jump" > Jumping to OS image. </CMD>

</LIST>

In cfg.ini, i replace name=Sabre-SD with

name = Sabre-SD-uBootOnly

In OS Firmware, i created empty u-boot.bin file

Sabrelite is connected through serial cable to USB.

run hyperterminal (115200, Data 8)

When i start MfgTool2.exe, below error appear

Monday, August 25, 2014 14:17:12   Start new logging

ModuleID[2] LevelID[1]: Boot command-- file[C:\imx6\New folder\Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\u-boot.bin] data buffer alloc failed

ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 3

0 件の賞賛
返信

5,534件の閲覧回数
chewhouming
Contributor III

Eric

I find this link very useful but where to get the file u-boot.imx

http://boundarydevices.com/windows-users-and-unbricking-an-i-mx-device/

0 件の賞賛
返信

5,534件の閲覧回数
EricNelson
Senior Contributor II

Hi Chew,

As of this writing, the latest U-Boot binaries are 2014.04:

     http://boundarydevices.com/u-boot-2014-04-release-mx6/

This URL is updated with each release:

     http://commondatastorage.googleapis.com/boundarydevices.com/u-boot-production.tar.gz

Regards,


Eric

0 件の賞賛
返信

5,534件の閲覧回数
chewhouming
Contributor III

hi

I paste the content in Linaro>OS Firmware into sbloader folder.

In command prompt, sb_loader.exe -f u-boot-mx6q-sabrelite.bin

Waiting for HID device for 2 seconds ..

HID device was not found.

Please place the device in recovery mode and restart the program.

I set boot switch to every location (00, 01), but not working

0 件の賞賛
返信

5,534件の閲覧回数
EricNelson
Senior Contributor II

Hi Chew,

Some boards had SW1 mounted backwards, so "10" or "01" could be the serial boot loader position.

In the right position, you should see Windows notify you of a new (unrecognized) device when power-cycled in the correct position. In other words, you don't need sb_loader to determine if the device is in the right mode.

If none of the position yields this result, something is wrong with either hardware or cabling. The serial boot loader mode needs almost nothing besides proper power, a functioning CPU, and good cabling to a host device.

Regards,


Eric

5,534件の閲覧回数
chewhouming
Contributor III

hi

From the link, i cannot find U-Boot 2012.10

http://boundarydevices.com/switching-u-boot-versions-on-i-mx6/

Please assist.

0 件の賞賛
返信

5,534件の閲覧回数
chewhouming
Contributor III

hi

i can't find

6q_upgrade-20121112.zip file

from the link


Freescale i.MX6 Development Platforms: Getting ... | element14


can you kindly direct me to uboot.imx, i think i am loss in this particular stage.

0 件の賞賛
返信

5,534件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chew

yes this is good link, it may answer your problem.

If not, please post on below

http://boundarydevices.com/community/

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信