SabreSD board - SD card preparation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SabreSD board - SD card preparation

1,191 Views
supriyac
Contributor I


Hello Team,

Am trying to boot sabresd board with the my compiled images. (uboot and kernel)

Could you please provide me with sd card preparation procedure?

Also am trying to get rootfs.tar via buildroot

Am facing two problems when following below link:

(Buildroot for the i.MX6 sabre sd platform in a few commands )

1. getting error during configuration as

make[1]: *** No rule to make target `freescale_imx6sabresd_defconfig'.  Stop.

2. Kernel not booting

mmc1 is current device

** Unrecognized filesystem type **

** Unrecognized filesystem type **

Booting from net ...

FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !

0 Kudos
Reply
2 Replies

677 Views
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to section 4.3 (Preparing an SD/MMC card to boot) of the "i.MX_Linux_User's_Guide.pdf"

of the recent NXP BSP (please use it) :

https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_MX6QDLSOLO&appType=license&location=null&...

Summary page :

i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

677 Views
supriyac
Contributor I

Thank you Yuri.

0 Kudos
Reply