SabreSD: Adding DCD item to u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SabreSD: Adding DCD item to u-boot

Jump to solution
1,928 Views
ts
Contributor II

Hi,

For testing adding a DCD Item, i modified flash_header.S to add one more DCD item to modify ENET_PALR, after the 83rd item (SabreSD, i.mx6Q):

MXC_DCD_ITEM(84, 0x021880E4, 0xFFFFFFFF)

I updated dcd_hdr and write_dcd_cmd as:

dcd_hdr:      .word 0x40a802D2
write_dcd_cmd:.word 0x04A402CC

The u-boot now fails to boot up.  If i modify the 84th DCD Item to be the same as the 83rd DCD item (i.e. configuring DDR) it works.

Are there limitations to what registers can be updated by the ROM from the DCD list, or am i missing something?

thanks

Labels (1)
1 Solution
1,394 Views
Yuri
NXP Employee
NXP Employee

Please look at Table 8-35 (Valid DCD Address Ranges) in i.MX6Q Reference Manual.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fpsp=1

View solution in original post

5 Replies
1,394 Views
fabio_estevam
NXP Employee
NXP Employee

Why exactly do you need to touch ENET_PALR from the DCD? What is the issue you are trying to solve?

0 Kudos
Reply
1,394 Views
RodBorras
NXP Employee
NXP Employee

Tarak,

You are only using 680 of the 1768 DCD bytes, so you should be fine.

But modifying the MAC address might have boot repercussions, especially if you are trying an NFS mount.

If your goal is to just modify some generic registers in the DCD, try something more benign. I do not see why you cannot change just about anything you want, in there.

Regards,

Rod.

0 Kudos
Reply
1,394 Views
ts
Contributor II

Rod,  apparently not all addresses can be accessed as indicated by Yuri's link to table 8-35.

0 Kudos
Reply
1,394 Views
RodBorras
NXP Employee
NXP Employee

Tarak: thank you for pointing this out to me, I was unaware of it.

Yuri: my apologies, I misunderstood your post, and did not realize it contained the answer.

0 Kudos
Reply
1,395 Views
Yuri
NXP Employee
NXP Employee

Please look at Table 8-35 (Valid DCD Address Ranges) in i.MX6Q Reference Manual.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fpsp=1