SabreLite and SabreSD HDMI output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SabreLite and SabreSD HDMI output

646 Views
andyclayton
Contributor I

We have a SabreLite board which outputs HDMI at 720p perfectly, however a SabreSD ( and a custom board) running the same code and outputting to the same monitor outputs video that seems to big for the screen, i.e the edges are cut off. Has anyone else seen this happen? The only difference I can see between the SabreSD and the SabreLite in the HDMI department is the SabreSD has an ESD device on the HDMI signals.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

523 Views
igorpadykov
NXP Employee
NXP Employee

Hi andy

what are full part numbers of processors on these boards ?

Reason may be that sabrelite boards used old rev.1.0 of i.MX6Q processor,

which is not supported currently on FSL BSPs.

Best regards

igor

0 Kudos
Reply