Sabre SD (MCIMX6Q-SDB) with L3.0.35_1.1.0 Linux BSP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabre SD (MCIMX6Q-SDB) with L3.0.35_1.1.0 Linux BSP?

1,543 Views
stevekwon
Contributor II

Hi,

I'm having issues getting the new L3.0.35_1.1.0 Linux BSP to even boot on my Sabre SDB board.  I've loaded uBoot and it doesn't seem to boot.  So I had to load uBoot from a older release.

I've then try to boot the kernel over SD, eMMC and TFTP, but they are all panicking at around the same point.

My question is, do you know if the BSP works with a Sabre SD board?

Also, do you know if 3D rendering inside Ubuntu is supported with this release?  So I could run a gl app such as glmark2 and get 3D acceleration?

Thanks.

Steve

Labels (4)
0 Kudos
Reply
2 Replies

853 Views
RodBorras
NXP Employee
NXP Employee

Hi Steve,

I have 2 Sabre SDBs, and 1 Sabre SDP, and they all run the L3.0.35_1.1.0 Linux BSP correctly.

I boot from SD, eMMC, and NFS, with no problems.

How did you create your SD card? Did you put u-boot.bin and uImage directly at the beginning of the card (just after the MBR, no partition), and the RFS in partition 1?

Did you create partition 1 deep enough into the SD card to avoid clipping the uImage (kernel)?

If you give us a few more details, we can help you.

Also, I have run many OpenGL 3D demos with the Min Profile version of this BSP. I would imagine the Ubuntu RFS can do the same.

Thanks,

Rod.

853 Views
PrabhuSundarara
NXP Employee
NXP Employee

I tried boot from SD, it worked good.

Also boot up with ubuntu filesystem and install

apt-get install mesa-utils

now run glxgears, you can see the GPU accelerated.