Sabre Board_Ethernet PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabre Board_Ethernet PHY

1,399 Views
hareeshth
Contributor I

Hi,

Is there any equivalent part for QUALCOMM ATHEROS AR8031-AL1B Module.

Regards,

Hareesh

Labels (1)
0 Kudos
Reply
1 Reply

1,069 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hareesh

AR8033 is a less expensive version of the AR8031 as it does not have the 1588 support.

However on web there has been some information that direct replacement leads

to link speed issues, so seems some modification of drivers needed.

Also other phy can be used, such as KSZ9021

http://boundarydevices.com/product/sabre-lite-imx6-sbc/?gclid=CKvP5PTSisgCFYQRHwodqdIOVw

broadcom phy

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply