Saberlite (now BD-imx6-sl) board freezes up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Saberlite (now BD-imx6-sl) board freezes up

ソリューションへジャンプ
2,219件の閲覧回数
sriramchadalava
Contributor III

I built an Android Jellybean image for Saberlite board that always causes the board to suspend soon after shell comes up on the console. If the imx2 watchdog timer driver is enabled, it always resets the board.

CONSOLE LOG

-------------------------

Linux version 3.0.35-ga7ddca5-dirty (ram@ram-Latitude-E6520) (gcc version 4.6.x3

---------------------------

---------------------------

---------------------------

request_suspend_state: sleep (0->3) at 42329537674 (1970-01-02 00:06:03.6991540)

PM: Syncing filesystems ... done.                                        
suspend: start 1 suspend...                                              
suspend: finish 1 suspend after:0.2542333 seconds...                     
Freezing user space processes ... (elapsed 0.01 seconds) done.           
Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.      
add wake up source irq 100                                               
add wake up source irq 51                                                
PM: suspend of devices complete after 122.410 msecs                      
PM: late suspend of devices complete after 0.686 msecs                   
Disabling non-boot CPUs ...                                              
CPU1: shutdown                                                           
CPU2: shutdown                                                           

CPU3: shutdown

Please let me know if you need more (log) information to figure out what the problem is.

And help me avoid/eliminate this behavior or at the very least, work around it.


Thanks.

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 解決策
1,808件の閲覧回数
maheshmahadeva1
NXP Employee
NXP Employee

Thanks for pointing this out, I have edited and added the link to my reply.

Best regards,

-Mahesh

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,808件の閲覧回数
YixingKong
Senior Contributor IV

Sriram, has your question been answered? If yes, please click Correct Answer/Helpful Answer.

Thanks,

Yixing

0 件の賞賛
返信
1,808件の閲覧回数
maheshmahadeva1
NXP Employee
NXP Employee

Please use the below link for issues and support related to MX6 Sabre-lite platform.

http://boundarydevices.com/products/sabre-lite-imx6-sbc/

Best regards,

-Mahesh

0 件の賞賛
返信
1,808件の閲覧回数
LeonardoSandova
Specialist I

Hi Manesh, I think the link is missing....

Leo

0 件の賞賛
返信
1,809件の閲覧回数
maheshmahadeva1
NXP Employee
NXP Employee

Thanks for pointing this out, I have edited and added the link to my reply.

Best regards,

-Mahesh

0 件の賞賛
返信