I built an Android Jellybean image for Saberlite board that always causes the board to suspend soon after shell comes up on the console. If the imx2 watchdog timer driver is enabled, it always resets the board.
CONSOLE LOG
-------------------------
Linux version 3.0.35-ga7ddca5-dirty (ram@ram-Latitude-E6520) (gcc version 4.6.x3
---------------------------
---------------------------
---------------------------
request_suspend_state: sleep (0->3) at 42329537674 (1970-01-02 00:06:03.6991540)
PM: Syncing filesystems ... done. | |
suspend: start 1 suspend... | |
suspend: finish 1 suspend after:0.2542333 seconds... | |
Freezing user space processes ... (elapsed 0.01 seconds) done. | |
Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done. | |
add wake up source irq 100 | |
add wake up source irq 51 | |
PM: suspend of devices complete after 122.410 msecs | |
PM: late suspend of devices complete after 0.686 msecs | |
Disabling non-boot CPUs ... | |
CPU1: shutdown | |
CPU2: shutdown |
CPU3: shutdown
Please let me know if you need more (log) information to figure out what the problem is.
And help me avoid/eliminate this behavior or at the very least, work around it.
Thanks.
解決済! 解決策の投稿を見る。
Thanks for pointing this out, I have edited and added the link to my reply.
Best regards,
-Mahesh
Sriram, has your question been answered? If yes, please click Correct Answer/Helpful Answer.
Thanks,
Yixing
Please use the below link for issues and support related to MX6 Sabre-lite platform.
http://boundarydevices.com/products/sabre-lite-imx6-sbc/
Best regards,
-Mahesh
Hi Manesh, I think the link is missing....
Leo
Thanks for pointing this out, I have edited and added the link to my reply.
Best regards,
-Mahesh