SX-SDCAN on IMX6Q yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SX-SDCAN on IMX6Q yocto

3,841 Views
morganmckenzie
Contributor I

Hi,

I don't know if anyone else has near the same configuration as me - but I've been trying to enable the SX-SDCAN module for my imx6q sabre auto board. I've searched google and come up with a few things but none resulting in a fix, and am going to contact the manufacturer to see if they can help.

I've built up an image based on core-image - I haven't configured the kernel but Atheros ath6kl support is enabled as a module. I've tried in dora, master, and master-next with the same results.

I was wondering if anyone has had experience with the SX-SDCAN under yocto (and more particularly success?)

During the board's boot cycle it gives the following messages:

ath6kl: Failed to get board file ath6k/AR6003/hw2.1.1/bdata.bin (-2), trying to find default board file.

ath6kl: Failed to get default board file ath6k/AR6003/hw2.1.1/bdata.SD31.bin: -2

ath6kl: Failed to init ath6kl core

ath6kl_sdio: probe of mmc1:0001:1 failed with error -2

And, these are the contents of /lib/firmware/ath6k/AR6003/hw2.1.1, so it seems to have the things I need there:

athwlan.bin
bdata.SD31.bin
bdata.SD32.bin
bdata.WB31.bin

bdata.bin -> bdata.SD31.bin
bdata.patch.bin
endpointpoing.bin
fw-2.bin
fw-3.bin
opt.bin

I've also tried copying over the hw2.1.1 and /lib/drivers/***/devices/net/kernel/ath.ko (that path might not be right, but it is in the device -  I don't currently have access to the computer or board) from the oneiric.tgz release on the freescale website.

Any help would be much appreciated!

Morgan McKenzie

0 Kudos
Reply
4 Replies

2,227 Views
andy_ross_silex
Contributor I

Morgan,

We are looking at this right now. I'll get the engineer looking at the Yocto release in the loop, he may have something he can share.

Andy Ross - Silex Technology America

0 Kudos
Reply

2,227 Views
KursadOney
NXP Employee
NXP Employee

Andrew,

I have the same problem too. Any updates? I'm running:

Linux imx6qsabresd 3.0.35-4.1.0+yocto+gbdde708 #1 SMP PREEMPT Mon Feb 3 15:06:42 EST 2014 armv7l GNU/Linux

Files:

root@imx6qsabresd:~# ls -al /lib/firmware/ath6k/AR6003/hw2.1.1

total 308

drwxr-xr-x 2 root root  4096 Feb 25  2014 .

drwxr-xr-x 5 root root  4096 Feb  3 21:38 ..

-rw-r--r-- 1 root root  68975 Feb  3 21:25 athwlan.bin

-rw-r--r-- 1 root root  1792 Feb  3 21:25 bdata.SD31.bin

-rw-r--r-- 1 root root  1792 Feb  3 21:25 bdata.SD32.bin

-rw-r--r-- 1 root root  1792 Feb  3 21:25 bdata.WB31.bin

-rw-r--r-- 1 root root  1792 Feb 25  2014 bdata.bin

-rw-r--r-- 1 root root    140 Feb  3 21:25 data.patch.bin

-rw-r--r-- 1 root root  12810 Feb  3 21:25 endpointping.bin

-rw-r--r-- 1 root root  89844 Feb  3 21:25 fw-2.bin

-rw-r--r-- 1 root root 104562 Feb  3 21:25 fw-3.bin

-rw-r--r-- 1 root root  2783 Feb  3 21:25 otp.bin

Error message:

ath6kl: Failed to get board file ath6k/AR6003/hw2.1.1/bdata.bin (-2), trying to find default board file.

ath6kl: Failed to get default board file ath6k/AR6003/hw2.1.1/bdata.SD31.bin: -2

ath6kl: Failed to init ath6kl core

ath6kl_sdio: probe of mmc2:0001:1 failed with error -2

0 Kudos
Reply

2,227 Views
morganmckenzie
Contributor I

Hi,

So I actually figured out what the issue was a week or so ago. It is actually something to do with the boot order in Yocto and nothing to do with the board file - if you rmmod ath6kl and modprobe ath6kl it should work just fine, given that you have a board file. I think it's that the os is trying to load the module before the filesystem is up, and therefore when it goes to read the board configuration file it can't. I'm trying to work on an actual solution for this but I really don't know yocto that well so I'm a bit out of my league.. I did manage to get it working with hacky solution shown below:

I added a file blacklist.conf in /etc/modprobe.d with the following line: install ath6kl /bin/false

and I added this line to one of the linux start files (I have it set up to run in S99):  modprobe --ignore-install ath6kl

I was wondering though Andrew - what is the possibility of getting updated firmware/board configuration file for the board? The download on the silex website really doesn't work - on this page it says to click the link to download but there is no link: SX-SDCAN | Radio Modules | Silex Technology America

0 Kudos
Reply

2,227 Views
jamesbone
NXP TechSupport
NXP TechSupport

andy_ross_silex do you get any luck to involve the engineer in charge?

0 Kudos
Reply