Hello,
We are planning to use EMMC08G-T227 or EMMC08G-MB29 eMMC in our design for a custom board based on IMX8M Mini Processor with Android 9 (p9.0.0_2.3.0).
I am looking through the SW code for these eMMC in the u-boot, but did not find any code specific for these eMMCs.
Are these eMMCs supported by the BSP U-boot by default without any changes?
Or does eMMC support require any specific software changes for adding support of these eMMC? If yes, please suggest the required changes.
Regards,
Naman
Solved! Go to Solution.
Hi namanthaker
for emmc parts no specific codes are needed as all these parts are handled
in the same way, according to emmc specifications as described in sect.10.3.1.1 Features
i.MX 8M Mini Applications Processor Reference Manual
Best regards
igor
Hi namanthaker
for emmc parts no specific codes are needed as all these parts are handled
in the same way, according to emmc specifications as described in sect.10.3.1.1 Features
i.MX 8M Mini Applications Processor Reference Manual
Best regards
igor