SVD file for i.MX28

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SVD file for i.MX28

742 次查看
alexlesuper
Contributor I

Hello,

I was wondering if the SVD XML file for the i.MX28 could be made available? I've tried looking on the ARM (https://cmsis.arm.com/vendor/freescale-semiconductor/ ) website and there are only MK device SVD files available. Having this file handy would greatly speed up my debugging and development process.

Thanks,

Alexandre Courtemanche

标签 (2)
0 项奖励
1 回复

583 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Alejexandre,

You are not going to find SVD file for the i.MX28 since it is an ARM926 Core, which means the only CMSIS-SVD files are for Cortex processors or Microcontrollers like the Kinetis family or the i.MX6 family.  In this case if you are using a DS-5 for debugging,  I think you only need to have the connection configuration using the proper script to initialize the device and that´s it.